JAJSBK7H January 2012 – February 2018 DS125DF410
PRODUCTION DATA.
The configuration mode is selected by the state of the SMBus Enable pin (pin 20) when the DS125DF410 is powered-up. This pin should be either left floating or tied to the device VDD through an optional 1kΩ resistor. The effect of each of these settings is shown in Table 4.
PIN
SETTING |
CONFIGURATION
MODE |
DESCRIPTION | READ_EN PIN |
---|---|---|---|
Float | SMBus Master Mode | Device reads its configuration from an external EEPROM on power-up. | Pull low to initiate reading configuration data from external EEPROM |
High (1) | SMBus Slave Mode | Device is configured over the SMBus by an external controller. | Tie low to enable proper address strapping on power-up |