JAJSSV1B December 2017 – January 2024 FPC202
PRODUCTION DATA
Writing data to an FPC202 device or the downstream ports under its management requires one SPI transactions. Multiple write transactions to downstream ports can proceed with minimal delay provided that different ports are being written to. If attempting to write data to the same downstream port, then the corresponding downstream access delay, tOFF-SSN, is required. Figure 7-12 shows an example of writing to both downstream ports in succession.