JAJSCM3E August 2006 – January 2021 INA193A-Q1 , INA194A-Q1 , INA195A-Q1 , INA196A-Q1 , INA197A-Q1 , INA198A-Q1
PRODUCTION DATA
Although the INA19xA-Q1 family of devices are not designed for accurate operation in either of these regions, some applications are exposed to these conditions; for example, when monitoring power supplies that are switched on and off while VS is still applied to the INA19xA-Q1. It is important to know what the behavior of the devices will be in these regions.
As VSENSE approaches 0 mV, in these
VCM regions, the device output accuracy degrades. A
larger-than-normal offset can appear at the current shunt monitor output with a
typical maximum value of VOUT = 300 mV for
VSENSE = 0 mV. As VSENSE approaches 20 mV, VOUT
returns to the expected output value with accuracy as specified in Electrical Characteristics. #SBOS400IMG1258 illustrates this effect using the INA195A and INA198A
(Gain = 100).