JAJSCW1C July 2016 – December 2016 INA260
PRODUCTION DATA.
Connections to the internal shunt resistor should be connected directly into and out of the shunt resistor pins to encourage uniform current flow through the device. The trace width should be sized correctly to handle the desired current flow. Place the power-supply bypass capacitor as close as possible to the supply and ground pins. Use of multiple vias to connect the device ground to the bypass capacitor grounds is recommended if there is not direct connection on the top layer.
NOTE:
Connect the VBUS pin to the power supply rail.