JAJSI63 November 2019 LDC1001-Q1
PRODUCTION DATA.
Rp_MIN sets the lower limit of the LDC1001-Q1 resonant impedance input range.
For example, if RP at 1 mm is measured to be 5 kΩ, 5000 / 2 = 2500. Referring to Table 4, 2.394 kΩ is the smallest value smaller than 2.5 kΩ, which corresponds to an Rp_MIN value of 0x3B.
Setting Rp_MIN to a value not listed on Table 4 can result in indeterminate behavior. In addition, Rp_MIN powers on with a default value of 0x14 which must be set to a value from Table 4 prior to powering on the LDC.