If certain faults are detected in the DIAGNOSTICS, NORMAL or FAULT state, the device transitions to the DISABLED state. These are the characteristics of the DISABLED state:
- The LC oscillator is disabled.
- The Analog Front End is disabled.
- The output stage is tri-stated and OUT pins are pulled up or down by external resistors to indicate the FAULT state.
The device transitions from the DISABLED state to one of the following:
- DIAGNOSTICS state after 20 ms to attempt recovery. For EEPROM CRC error, the device will only attempt recovery three times.
- The device transitions to the IDLE state upon power cycle.