JAJSBH5B March 2011 – June 2019 LM21212-2
PRODUCTION DATA.
The PGOOD pin provides the user with a way to monitor the status of the LM21212-2. In order to use the PGOOD pin, the application must provide a pullup resistor to a desired DC voltage (in other words, VIN). PGOOD responds to a fault condition by pulling the PGOOD pin low with the open-drain output. PGOOD will pull low on the following conditions – 1) VFB moves above or below the VOVP or VUVP, respectively 2) The enable pin is brought below the enable threshold 3) The device enters a prebiased output condition (VFB>VSS).
Figure 19 shows the conditions that will cause PGOOD to fall.