JAJSVG8 October 2024 LM251772
PRODUCTION DATA
The VCC2 regulator is the supply for the integrated gate driver. The LDO starts in low-current, pre-bias mode, once the voltage on the nRST-Pin is higher that its rising threshold. If the EN/UVLO pin is higher that its rising threshold the VCC2 is fully active and provides the target performance specified by the electrical characteristics parameters.
It is not recommended to connect an external load to the VCC2-PIN