JAJS933L September 1998 – June 2016 LM2672
PRODUCTION DATA.
The input voltage for the power supply is connected to the VIN pin. In addition to providing energy to the load the input voltage also provides bias for the internal circuitry of the LM2672. For ensured performance, the input voltage must be in the range of 6.5 V to 40 V. For best performance of the power supply, the VIN pin must always be bypassed with an input capacitor placed close to this pin and GND.