JAJSA07F November   2002  – October 2016 LM2705

PRODUCTION DATA.  

  1. 特長
  2. アプリケーション
  3. 概要
  4. 改訂履歴
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
    6. 6.6 Typical Characteristics
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
        1. 8.2.2.1 Inductor Selection - Boost Regulator
        2. 8.2.2.2 Inductor Selection - SEPIC Regulator
        3. 8.2.2.3 Diode Selection
        4. 8.2.2.4 Capacitor Selection
      3. 8.2.3 Application Curves
    3. 8.3 Additional Applications
  9. Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
  11. 11デバイスおよびドキュメントのサポート
    1. 11.1 デバイス・サポート
      1. 11.1.1 Third-Party Products Disclaimer
    2. 11.2 ドキュメントの更新通知を受け取る方法
    3. 11.3 コミュニティ・リソース
    4. 11.4 商標
    5. 11.5 静電気放電に関する注意事項
    6. 11.6 Glossary
  12. 12メカニカル、パッケージ、および注文情報

パッケージ・オプション

メカニカル・データ(パッケージ|ピン)
サーマルパッド・メカニカル・データ
発注情報

Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

Application Information

The LM2705 is a 20-V boost designed for low power boost applications. Typical input voltage range makes this ideal for standard single cell Li+ batteries or 2 to 4 series alkaline batteries.

Typical Application

Figure 12 shows a typical Li+ voltage range to 20-V application. The 68-µH inductor allows for a low ripple current and high light-load efficiency.

LM2705 20039701.gif Figure 12. Typical 20-V Application

Design Requirements

For typical DC-DC converter applications, use the parameters listed in Table 1.

Table 1. Design Parameters

DESIGN PARAMETER EXAMPLE VALUE
Input voltage 2.5 V to 4.2 V
Output voltage 12 V
Output current up to 8 mA
Inductor 33 µH

Detailed Design Procedure

Inductor Selection - Boost Regulator

The appropriate inductor for a given application is calculated using Equation 1:

Equation 1. LM2705 20039707.gif

where

  • VD is the Schottky diode voltage
  • ICL is the switch current limit found in the Typical Characteristics
  • TOFF is the switch off time

When using this equation be sure to use the minimum input voltage for the application, such as for battery powered applications. For the LM2705 constant-off time control scheme, the NMOS power switch is turned off when the current limit is reached. There is approximately a 100-ns delay from the time the current limit is reached in the NMOS power switch and when the internal logic actually turns off the switch. During this 100-ns delay, the peak inductor current increases. This increase in inductor current demands a larger saturation current rating for the inductor. This saturation current can be approximated by Equation 2:

Equation 2. LM2705 20039708.gif

Choosing inductors with low ESR decrease power losses and increase efficiency.

Take care when choosing an inductor. For applications that require an input voltage that approaches the output voltage, such as when converting a Li-Ion battery voltage to 5 V, the 400-ns off time may not be enough time to discharge the energy in the inductor and transfer the energy to the output capacitor and load. This can cause a ramping effect in the inductor current waveform and an increased ripple on the output voltage. Using a smaller inductor causes the IPK to increase and increases the output voltage ripple further.

For typical curves and evaluation purposes the DT1608C series inductors from Coilcraft were used. Other acceptable inductors include, but are not limited to, the SLF6020T series from TDK, the NP05D series from Taiyo Yuden, the CDRH4D18 series from Sumida, and the P1166 series from Pulse.

Inductor Selection - SEPIC Regulator

Equation 3 can be used to calculate the approximate inductor value for a SEPIC regulator:

Equation 3. LM2705 20039744.gif

The boost inductor, L1, can be smaller or larger but is generally chosen to be the same value as L2. See Figure 23 and Figure 24 for typical SEPIC applications.

Diode Selection

To maintain high efficiency, the average current rating of the Schottky diode should be larger than the peak inductor current, IPK. Schottky diodes with a low forward drop and fast switching speeds are ideal for increasing efficiency in portable applications. Choose a reverse breakdown of the Schottky diode larger than the output voltage.

Capacitor Selection

Choose low equivalent series resistance (ESR) capacitors for the output to minimize output voltage ripple. Multilayer ceramic capacitors are the best choice. For most applications, a 1-µF ceramic capacitor is sufficient. For some applications a reduction in output voltage ripple can be achieved by increasing the output capacitor. Output voltage ripple can further be reduced by adding a 4.7-pF feed-forward capacitor in the feedback network placed in parallel with RF1 (see Functional Block Diagram).

Local bypassing for the input is needed on the LM2705. Multilayer ceramic capacitors are a good choice for this as well. A 4.7-µF capacitor is sufficient for most applications. For additional bypassing, a 100-nF ceramic capacitor can be used to shunt high frequency ripple on the input.

Application Curves

LM2705 20039724.png
Figure 13. Efficiency vs Load Current
LM2705 20039749.png
Figure 15. Output Ripple Voltage
Copt, Ropt Included
LM2705 20039743.png Figure 17. Two White-LED Efficiency
LM2705 20039725.png
Figure 14. Efficiency vs Load Current
LM2705 20039750.png
Figure 16. Output Ripple Voltage
Copt, Ropt Excluded
LM2705 20039742.png Figure 18. Three White-LED Efficiency

Additional Applications

LM2705 20039709.gif Figure 19. Two White-LED Application
LM2705 20039734.gif Figure 20. Three White-LED Application
LM2705 20039735.gif Figure 21. Li-Ion 12-V Application
LM2705 20039736.gif Figure 22. 5-V to 12-V Application
LM2705 20039739.gif Figure 23. 3.3-V SEPIC Application
LM2705 20039740.gif Figure 24. 5-V SEPIC Application