JAJSA73K September 2004 – September 2018 LM2734
PRODUCTION DATA.
Input voltage is rated as 3 V to 18 V; however, care must be taken in certain circuit configurations (for example, VBOOST derived from VIN where the requirement that VBOOST – VSW < 5.5 V should be observed) Also, for best efficiency VBOOST should be at least 2.5-V above VSW.
The voltage on the Enable pin should not exceed VIN by more than 0.3 V.