JAJSA67I April 2004 – February 2019 LM2743
PRODUCTION DATA.
The following is a sample calculation.
A reasonable estimation of the efficiency of a switching buck controller can be obtained by adding together the Output Power (POUT) loss and the Total Power (PTOTAL) loss:
The Output Power (POUT) for the Figure 30 design is (1.2 V x 4 A) = 4.8 W. The Total Power (PTOTAL), with an efficiency calculation to complement the design, is shown below.
The majority of the power losses are due to low and high side of MOSFET’s losses. The losses in any MOSFET are group of switching (PSW) and conduction losses(PCND).
The following equations show FET Switching Loss (PSW).
The FDS6898A has a typical turn-on rise time tr and turn-off fall time tf of 15 ns and 16 ns, respectively. The switching losses for this type of dual N-Channel MOSFETs are 0.061 W.
The following equations show FET Conduction Loss (PCND).
RDS(ON) = 13 mΩ and the factor is a constant value (k = 1.3) to account for the increasing RDS(ON) of a FET due to heating.
There are few additional losses that are taken into account:
The following equations show IC Operating Loss (PIC).
where IQ-VCC is the typical operating VCC current
The following equations show FET Gate Charging Loss (PGATE).
The value n is the total number of FETs used and QGS is the typical gate-source charge value, which is 3 nC. For the FDS6898A the gate charging loss is 5.94 mW.
The following equations show Input Capacitor Loss (PCAP).
Here n is the number of paralleled capacitors, ESR is the equivalent series resistance of each, and PCAP is the dissipation in each. So for example if we use only one input capacitor of 24 mΩ.
The following equation shows Output Inductor Loss (PIND).
where DCR is the DC resistance. Therefore, for example
The following equations show Total System Efficiency.