SNVS422D August 2006 – September 2015 LM2831
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The LM2831 device will operate with input voltage range from 3 V to 5.5 V and provide a regulated output voltage. This device is optimized for high-efficiency operation with minimum number of external components. For component selection, see Detailed Design Procedure.
The device must be able to operate at any voltage within the recommended operating range. Load current must be defined to properly size the inductor, input, and output capacitors. Inductor should be able to handle full expected load current as well as the peak current generated during load transients and start up. Inrush current at start-up will depend on the output capacitor selection. More details are provided in Detailed Design Procedure.
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831X |
C1, Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Cap | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1 | 3.3 µH, 2.2 A | TDK | VLCF5020T-3R3N2R0-1 |
R2 | 15.0 kΩ, 1% | Vishay | CRCW08051502F |
R1 | 15.0 kΩ, 1% | Vishay | CRCW08051502F |
R3 | 100 kΩ, 1% | Vishay | CRCW08051003F |
The duty cycle (D) can be approximated quickly using the ratio of output voltage (VO) to input voltage (VIN):
The catch diode (D1) forward voltage drop and the voltage drop across the internal PMOS must be included to calculate a more accurate duty cycle. Calculate D by using the following formula:
VSW can be approximated by:
The diode forward drop (VD) can range from 0.3 V to 0.7 V depending on the quality of the diode. The lower the VD, the higher the operating efficiency of the converter. The inductor value determines the output ripple current. Lower inductor values decrease the size of the inductor, but increase the output ripple current. An increase in the inductor value will decrease the output ripple current.
One must ensure that the minimum current limit (1.8 A) is not exceeded, so the peak current in the inductor must be calculated. The peak current (ILPK) in the inductor is calculated by:
In general,
If ΔiL = 20% of 1.50 A, the peak current in the inductor will be 1.8 A. The minimum ensured current limit over all operating conditions is 1.8 A. One can either reduce ΔiL, or make the engineering judgment that zero margin will be safe enough. The typical current limit is 2.5 A.
The LM2831 operates at frequencies allowing the use of ceramic output capacitors without compromising transient response. Ceramic capacitors allow higher inductor ripple without significantly increasing output ripple. See the Output Capacitor section for more details on calculating output voltage ripple. Now that the ripple current is determined, the inductance is calculated by:
Where:
When selecting an inductor, make sure that it is capable of supporting the peak output current without saturating. Inductor saturation will result in a sudden reduction in inductance and prevent the regulator from operating correctly. Because of the speed of the internal current limit, the peak current of the inductor need only be specified for the required maximum output current. For example, if the designed maximum output current is 1 A and the peak current is 1.25 A, then the inductor should be specified with a saturation current limit of > 1.25 A. There is no need to specify the saturation or peak current of the inductor at the 2.5-A typical switch current limit. The difference in inductor size is a factor of 5. Because of the operating frequency of the LM2831, ferrite based inductors are preferred to minimize core losses. This presents little restriction since the variety of ferrite-based inductors is huge. Lastly, inductors with lower series resistance (RDCR) will provide better operating efficiency. For recommended inductors, see LM2831X Design Example 2 through LM2831X Buck Converter and Voltage Double Circuit With LDO Follower Design Example 9.
An input capacitor is necessary to ensure that VIN does not drop excessively during switching transients. The primary specifications of the input capacitor are capacitance, voltage, RMS current rating, and ESL (Equivalent Series Inductance). The recommended input capacitance is 22 µF. The input voltage rating is specifically stated by the capacitor manufacturer. Make sure to check any recommended deratings and also verify if there is any significant change in capacitance at the operating input voltage and the operating temperature. The input capacitor maximum RMS input current rating (IRMS-IN) must be greater than:
Neglecting inductor ripple simplifies the above equation to:
It can be shown from the above equation that maximum RMS capacitor current occurs when D = 0.5. Always calculate the RMS at the point where the duty cycle D is closest to 0.5. The ESL of an input capacitor is usually determined by the effective cross sectional area of the current path. A large leaded capacitor will have high ESL and a 0805 ceramic chip capacitor will have very low ESL. At the operating frequencies of the LM2831, leaded capacitors may have an ESL so large that the resulting impedance (2πfL) will be higher than that required to provide stable operation. As a result, surface mount capacitors are strongly recommended.
Sanyo POSCAP, Tantalum or Niobium, Panasonic SP, and multilayer ceramic capacitors (MLCC) are all good choices for both input and output capacitors and have very low ESL. For MLCCs it is recommended to use X7R or X5R type capacitors due to their tolerance and temperature characteristics. Consult capacitor manufacturer data sheets to see how rated capacitance varies over operating conditions.
The output capacitor is selected based upon the desired output ripple and transient response. The initial current of a load transient is provided mainly by the output capacitor. The output ripple of the converter is:
When using MLCCs, the ESR is typically so low that the capacitive ripple may dominate. When this occurs, the output ripple will be approximately sinusoidal and 90° phase shifted from the switching action. Given the availability and quality of MLCCs and the expected output voltage of designs using the LM2831, there is really no need to review any other capacitor technologies. Another benefit of ceramic capacitors is their ability to bypass high frequency noise. A certain amount of switching edge noise will couple through parasitic capacitances in the inductor to the output. A ceramic capacitor will bypass this noise while a tantalum will not. Since the output capacitor is one of the two external components that control the stability of the regulator control loop, most applications will require a minimum of 22 µF of output capacitance. Capacitance often, but not always, can be increased significantly with little detriment to the regulator stability. Like the input capacitor, recommended multilayer ceramic capacitors are X7R or X5R types.
The catch diode (D1) conducts during the switch off-time. A Schottky diode is recommended for its fast switching times and low forward voltage drop. The catch diode should be chosen so that its current rating is greater than:
The reverse breakdown rating of the diode must be at least the maximum input voltage plus appropriate margin. To improve efficiency, choose a Schottky diode with a low forward voltage drop.
The output voltage is set using the following equation where R2 is connected between the FB pin and GND, and R1 is connected between VO and the FB pin. A good value for R2 is 10 kΩ. When designing a unity gain converter (Vo = 0.6 V), R1 should be from 0 Ω to 100 Ω, and R2 should be equal or greater than 10 kΩ.
VIN = 5 V | VO = 1.8 V and 3.3 V |
VIN = 5 V | VO = 1.8 V and 3.3 V |
VIN = 5 V | VO = 1.8 V and 3.3 V |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831X |
C1, Input Capacitor | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Capacitor | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1 | 3.3 µH, 2.2 A | TDK | VLCF5020T- 3R3N2R0-1 |
R2 | 10.0 kΩ, 1% | Vishay | CRCW08051000F |
R1 | 0 Ω | ||
R3 | 100 kΩ, 1% | Vishay | CRCW08051003F |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831X |
C1, Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Cap | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1 | 2.7 µH 2.3 A | TDK | VLCF5020T-2R7N2R2-1 |
R2 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
R1 | 45.3 kΩ, 1% | Vishay | CRCW08054532F |
R3 | 100 kΩ, 1% | Vishay | CRCW08051003F |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831Y |
C1, Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Cap | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1 | 4.7 µH 2.1 A | TDK | SLF7045T-4R7M2R0-PF |
R1 | 45.3 kΩ, 1% | Vishay | CRCW080545K3FKEA |
R2 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831Y |
C1, Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Cap | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1 | 6.8 µH 1.8 A | TDK | SLF7045T-6R8M1R7 |
R1 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
R2 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831Z |
C1, Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Cap | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1 | 1.6 µH 2.0 A | TDK | VLCF4018T-1R6N1R7-2 |
R2 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
R1 | 45.3 kΩ, 1% | Vishay | CRCW08054532F |
R3 | 100 kΩ, 1% | Vishay | CRCW08051003F |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831Z |
C1, Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Cap | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1 | 1.6 µH, 2.0 A | TDK | VLCF4018T- 1R6N1R7-2 |
R2 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
R1 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
R3 | 100 kΩ, 1% | Vishay | CRCW08051003F |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1, U2 | 1.5-A Buck Regulator | TI | LM2831X |
U3 | Power on Reset | TI | LP3470M5X-3.08 |
C1, C3 Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, C4 Output Cap | 2x22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C7 | Trr delay capacitor | TDK | |
D1, D2 Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
L1, L2 | 3.3 µH, 2.2 A | TDK | VLCF5020T-3R3N2R0-1 |
R2, R4, R5 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |
R1, R6 | 45.3 kΩ, 1% | Vishay | CRCW08054532F |
R3 | 100 kΩ, 1% | Vishay | CRCW08051003F |
PART ID | PART VALUE | MANUFACTURER | PART NUMBER |
---|---|---|---|
U1 | 1.5-A Buck Regulator | TI | LM2831X |
U2 | 200-mA LDO | TI | LP2986-5.0 |
C1, Input Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C2, Output Cap | 22 µF, 6.3 V, X5R | TDK | C3216X5ROJ226M |
C3 – C6 | 2.2 µF, 6.3 V, X5R | TDK | C1608X5R0J225M |
D1, Catch Diode | 0.3 Vf Schottky 1.5 A, 30 VR | TOSHIBA | CRS08 |
D2 | 0.4 Vf Schottky 20 VR, 500 mA | ON Semi | MBR0520 |
L2 | 10 µH, 800 mA | CoilCraft | ME3220-103 |
L1 | 3.3 µH, 2.2 A | TDK | VLCF5020T-3R3N2R0-1 |
R2 | 45.3 kΩ, 1% | Vishay | CRCW08054532F |
R1 | 10.0 kΩ, 1% | Vishay | CRCW08051002F |