JAJSAY1E March 2008 – October 2017 LM2854
PRODUCTION DATA.
The LM2854 preserves flexibility by integrating the control components around the error amplifier while using three small external compensation components from VOUT to FB. An integrated type II (two pole, one zero) voltage-mode compensation network is featured. To ensure stability, an external resistor and small value capacitor can be added across the upper feedback resistor as a pole-zero pair to complete a type III (three pole, two zero) compensation network. For correct selection of these components, see Detailed Design Procedure.