JAJSFJ3L May 2003 – August 2023 LM2903-Q1 , LM2903B-Q1
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
Output current is determined by the load/pull-up resistance and logic/pull-up voltage. The output current will produce a output low voltage (VOL) from the comparator. In which VOL is proportional to the output current. Use Figure 3-5 to determine VOL based on the output current.
The output current can also effect the transient response. More will be explained in the next section.