JAJSDE1 June   2017 LM317-N-MIL

PRODUCTION DATA.  

  1. 特長
  2. アプリケーション
  3. 概要
  4. 改訂履歴
  5. Pin Configuration and Functions
  6. Specifications
    1. 6.1 Absolute Maximum Ratings
    2. 6.2 ESD Ratings
    3. 6.3 Recommended Operating Conditions
    4. 6.4 Thermal Information
    5. 6.5 Electrical Characteristics
    6. 6.6 Typical Characteristics
  7. Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Load Regulation
    4. 7.4 Device Functional Modes
      1. 7.4.1 External Capacitors
      2. 7.4.2 Protection Diodes
  8. Application and Implementation
    1. 8.1 Application Information
    2. 8.2 Typical Applications
      1. 8.2.1  1.25-V to 25-V Adjustable Regulator
        1. 8.2.1.1 Design Requirements
        2. 8.2.1.2 Detailed Design Procedure
        3. 8.2.1.3 Application Curve
      2. 8.2.2  5-V Logic Regulator With Electronic Shutdown
      3. 8.2.3  Slow Turnon 15-V Regulator
      4. 8.2.4  Adjustable Regulator With Improved Ripple Rejection
      5. 8.2.5  High Stability 10-V Regulator
      6. 8.2.6  High-Current Adjustable Regulator
      7. 8.2.7  Emitter-Follower Current Amplifier
      8. 8.2.8  1-A Current Regulator
      9. 8.2.9  Common-Emitter Amplifier
      10. 8.2.10 Low-Cost 3-A Switching Regulator
      11. 8.2.11 Current-Limited Voltage Regulator
      12. 8.2.12 Adjusting Multiple On-Card Regulators With Single Control
      13. 8.2.13 AC Voltage Regulator
      14. 8.2.14 12-V Battery Charger
      15. 8.2.15 Adjustable 4-A Regulator
      16. 8.2.16 Current-Limited 6-V Charger
      17. 8.2.17 Digitally Selected Outputs
  9. Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
    3. 10.3 Thermal Considerations
      1. 10.3.1 Heatsink Requirements
      2. 10.3.2 Heatsinking Surface Mount Packages
        1. 10.3.2.1 Heatsinking the SOT-223 (DCY) Package
        2. 10.3.2.2 Heatsinking the TO-263 (KTT) Package
        3. 10.3.2.3 Heatsinking the TO-252 (NDP) Package
  11. 11デバイスおよびドキュメントのサポート
    1. 11.1 ドキュメントのサポート
      1. 11.1.1 関連資料
    2. 11.2 関連リンク
    3. 11.3 コミュニティ・リソース
    4. 11.4 商標
    5. 11.5 静電気放電に関する注意事項
    6. 11.6 Glossary
  12. 12メカニカル、パッケージ、および注文情報

パッケージ・オプション

メカニカル・データ(パッケージ|ピン)
サーマルパッド・メカニカル・データ
発注情報

Layout

Layout Guidelines

Some layout guidelines must be followed to ensure proper regulation of the output voltage with minimum noise. Traces carrying the load current must be wide to reduce the amount of parasitic trace inductance and the feedback loop from VOUT to ADJ must be kept as short as possible. To improve PSRR, a bypass capacitor can be placed at the ADJ pin and must be located as close as possible to the IC. In cases when VIN shorts to ground, an external diode must be placed from VOUT to VIN to divert the surge current from the output capacitor and protect the IC. Similarly, in cases when a large bypass capacitor is placed at the ADJ pin and VOUT shorts to ground, an external diode must be placed from ADJ to VOUT to provide a path for the bypass capacitor to discharge. These diodes must be placed close to the corresponding IC pins to increase their effectiveness.

Layout Example

LM317-N-MIL LM317-SOT223-layoutexample.png Figure 36. Layout Example (SOT-223)
LM317-N-MIL LM317-TO220-layoutexample.png Figure 37. Layout Example (TO-220)

Thermal Considerations

Heatsink Requirements

The LM317-N-MIL regulators have internal thermal shutdown to protect the device from over-heating. Under all operating conditions, the junction temperature of the LM317-N-MIL must not exceed the rated maximum junction temperature (TJ) of 125°C. A heatsink may be required depending on the maximum device power dissipation and the maximum ambient temperature of the application. To determine if a heatsink is needed, the power dissipated by the regulator, PD, must be calculate with Equation 3:

Equation 3. PD = ((VIN − VOUT) × IL) + (VIN × IG)

Figure 38 shows the voltage and currents which are present in the circuit.

The next parameter which must be calculated is the maximum allowable temperature rise, TR(MAX) in Equation 4:

Equation 4. TR(MAX) = TJ(MAX) − TA(MAX)

where TJ(MAX) is the maximum allowable junction temperature (125°C for the LM317-N-MIL), and TA(MAX) is the maximum ambient temperature that will be encountered in the application.

Using the calculated values for TR(MAX) and PD, the maximum allowable value for the junction-to-ambient thermal resistance (θJA) can be calculated with Equation 5:

Equation 5. θJA = (TR(MAX) / PD)
LM317-N-MIL 906360.gif Figure 38. Power Dissipation Diagram

If the calculated maximum allowable thermal resistance is higher than the actual package rating, then no additional work is needed. If the calculated maximum allowable thermal resistance is lower than the actual package rating either the power dissipation (PD) needs to be reduced, the maximum ambient temperature TA(MAX) needs to be reduced, the thermal resistance (θJA) must be lowered by adding a heatsink, or some combination of these.

If a heatsink is needed, the value can be calculated from Equation 6:

Equation 6. θHA ≤ (θJA – (θCH + θJC))

where

  • θCH is the thermal resistance of the contact area between the device case and the heatsink surface
  • θJC is thermal resistance from the junction of the die to surface of the package case

When a value for θHA is found using the equation shown, a heatsink must be selected that has a value that is less than, or equal to, this number.

The θHA rating is specified numerically by the heatsink manufacturer in the catalog, or shown in a curve that plots temperature rise vs power dissipation for the heatsink.

Heatsinking Surface Mount Packages

The TO-263 (KTT), SOT-223 (DCY) and TO-252 (NDP) packages use a copper plane on the PCB and the PCB itself as a heatsink. To optimize the heat sinking ability of the plane and PCB, solder the tab of the package to the plane.

Heatsinking the SOT-223 (DCY) Package

Figure 39 and Figure 40 show the information for the SOT-223 package. Figure 40 assumes a θJA of 74°C/W for 1-oz. copper and 59.6°C/W for 2-oz. copper and a maximum junction temperature of 125°C. See AN-1028 (SNVA036) for thermal enhancement techniques to be used with SOT-223 and TO-252 packages.

LM317-N-MIL 906357.gif Figure 39. θJA vs Copper (2-oz.) Area for the SOT-223 Package
LM317-N-MIL 906358.gif Figure 40. Maximum Power Dissipation vs TAMB for the SOT-223 Package

Heatsinking the TO-263 (KTT) Package

Figure 41 shows for the TO-263 the measured values of θJA for different copper area sizes using a typical PCB with 1-oz. copper and no solder mask over the copper area used for heatsinking.

As shown in Figure 41, increasing the copper area beyond 1 square inch produces very little improvement. It must also be observed that the minimum value of θJA for the TO-263 package mounted to a PCB is 32°C/W.

LM317-N-MIL 906355.png Figure 41. θJA vs Copper (1-oz.) Area for the TO-263 Package

As a design aid, Figure 42 shows the maximum allowable power dissipation compared to ambient temperature for the TO-263 device (assuming θJA is 35°C/W and the maximum junction temperature is 125°C).

LM317-N-MIL 906356.png Figure 42. Maximum Power Dissipation vs TAMB for the TO-263 Package

Heatsinking the TO-252 (NDP) Package

If the maximum allowable value for θJA is found to be ≥ 54°C/W (typical rated value) for the TO-252 package, no heatsink is needed because the package alone will dissipate enough heat to satisfy these requirements. If the calculated value for θJA falls below these limits, a heatsink is required.

As a design aid, Table 1 shows the value of the θJA of NDP the package for different heatsink area. The copper patterns that we used to measure these θJAs are shown in Figure 47. Figure 43 reflects the same test results as what are in Table 1.

Figure 44 shows the maximum allowable power dissipation versus ambient temperature for the TO-252 device. Figure 45 shows the maximum allowable power dissipation versus copper area (in2) for the TO-252 device. See AN-1028 (SNVA036) for thermal enhancement techniques to be used with SOT-223 and TO-252 packages.

Table 1. θJA Different Heatsink Area

LAYOUT COPPER AREA THERMAL RESISTANCE
Top Side (in2)(1) Bottom Side (in2) JA°C/W) TO-252
1 0.0123 0 103
2 0.066 0 87
3 0.3 0 60
4 0.53 0 54
5 0.76 0 52
6 1.0 0 47
7 0.066 0.2 84
8 0.066 0.4 70
9 0.066 0.6 63
10 0.066 0.8 57
11 0.066 1.0 57
12 0.066 0.066 89
13 0.175 0.175 72
14 0.284 0.284 61
15 0.392 0.392 55
16 0.5 0.5 53
Tab of device attached to topside of copper.
LM317-N-MIL 906361.gif Figure 43. θJA vs 2-oz. Copper Area for TO-252
LM317-N-MIL 906362.gif Figure 45. Maximum Allowable Power Dissipation vs 2-oz. Copper Area for TO-252
LM317-N-MIL 906363.gif Figure 44. Maximum Allowable Power Dissipation vs Ambient Temperature for TO-252
LM317-N-MIL 906364.gif Figure 46. Top View of the Thermal Test Pattern in Actual Scale
LM317-N-MIL 906365.gif Figure 47. Bottom View of the Thermal Test Pattern in Actual Scale