JAJSAI3C October 2006 – December 2016 LM3405
PRODUCTION DATA.
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | BOOST | O | Boost voltage that drives the NMOS output switch. A bootstrap capacitor is connected between the BOOST and SW pins. |
2 | GND | — | Signal and power ground pin. Place the bottom resistor of the feedback network as close as possible to this pin. |
3 | FB | I | Feedback pin. Connect FB to the LED string cathode and an external resistor to ground to set the LED current. |
4 | EN/DIM | I | Enable control input. Logic high enables operation. Toggling this pin with a periodic logic square wave of varying duty cycle at different frequencies controls the brightness of LEDs. Do not allow this pin to float or be greater than VIN + 0.3 V. |
5 | VIN | I | Input supply voltage. Connect a bypass capacitor locally from this pin to GND. |
6 | SW | O | Switch pin. Connect this pin to the inductor, catch diode, and bootstrap capacitor. |