JAJSAI3C October 2006 – December 2016 LM3405
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The duty cycle (D) can be approximated quickly using the ratio of output voltage (VOUT) to input voltage (VIN) in Equation 11.
The catch diode (D1) forward voltage drop and the voltage drop across the internal NMOS must be included to calculate a more accurate duty cycle. Calculate D by using Equation 12.
VSW can be approximated by Equation 13.
The diode forward drop (VD1) can range from 0.3 V to 0.7 V depending on the quality of the diode. The lower VD1 is, the higher the operating efficiency of the converter.
The inductor value determines the output ripple current (ΔiL, as defined in Figure 11). Lower inductor values decrease the size of the inductor, but increases the output ripple current. An increase in the inductor value decreases the output ripple current. The ratio of ripple current to LED current is optimized when it is set between 0.3 and 0.4 at 1A LED current. This ratio r is defined as:
One must also ensure that the minimum current limit (1.2 A) is not exceeded, so the peak current in the inductor must be calculated. The peak current (ILPK) in the inductor is calculated with Equation 15.
When the designed maximum output current is reduced, the ratio (r) can be increased. At a current of 0.2 A,
r can be made as high as 0.7. The ripple ratio can be increased at lighter loads because the net ripple is actually quite low, and if r remains constant the inductor value can be made quite large. An equation empirically developed for the maximum ripple ratio at any current below 2 A is calculated with Equation 16 (note that this is just a guideline).
The LM3405 operates at a high frequency allowing the use of ceramic output capacitors without compromising transient response. Ceramic capacitors allow higher inductor ripple without significantly increasing LED current ripple. See the output capacitor and feed-forward capacitor sections for more details on LED current ripple.
Now that the ripple current or ripple ratio is determined, the inductance is calculated by Equation 17.
where
When selecting an inductor, make sure that it is capable of supporting the peak output current without saturating. Inductor saturation results in a sudden reduction in inductance and prevent the regulator from operating correctly. Because of the operating frequency of the LM3405, ferrite based inductors are preferred to minimize core losses. This presents little restriction, because the variety of ferrite based inductors is huge. Lastly, inductors with lower series resistance (DCR) provides better operating efficiency. For recommended inductor selection, see Circuit Examples and Recommended Inductance Range in Table 1.
IF | INDUCTANCE RANGE AND INDUCTOR CURRENT RIPPLE | |||
---|---|---|---|---|
1 A | 4.7 µH TO 10 µH | |||
Inductance | 4.7 µH | 6.8 µH | 10 µH | |
ΔiL / IF(1) | 51% | 35% | 24% | |
0.6 A | 6.8 µH TO 15 µH | |||
Inductance | 6.8 µH | 10 µH | 15 µH | |
ΔiL / IF(1) | 58% | 40% | 26% | |
0.2 A | 4.7 µH(2) TO 22 µH | |||
Inductance | 10 µH | 15 µH | 22 µH | |
ΔiL / IF(1) | 119% | 79% | 54% |
An input capacitor is necessary to ensure that VIN does not drop excessively during switching transients. The primary specifications of the input capacitor are capacitance, voltage rating, RMS current rating, and ESL (Equivalent Series Inductance). The input voltage rating is specifically stated by the capacitor manufacturer. Check any recommended deratings and also verify if there is any significant change in capacitance at the operating input voltage and the operating temperature. The input capacitor maximum RMS input current rating (IRMS-IN) must be greater than Equation 18.
Equation 18 shows that maximum RMS capacitor current occurs when D = 0.5. Always calculate the RMS at the point where the duty cycle D, is closest to 0.5. The ESL of an input capacitor is usually determined by the effective cross sectional area of the current path. A large-leaded capacitor has high ESL and an 0805 ceramic chip capacitor has very low ESL. At the operating frequency of the LM3405, certain capacitors may have an ESL so large that the resulting inductive impedance (2 πfL) is higher than that required to provide stable operation. TI strongly recommends using ceramic capacitors due to their low ESR and low ESL. A 10-µF multilayer ceramic capacitor (MLCC) is a good choice for most applications. In cases where large capacitance is required, use surface mount capacitors such as Tantalum capacitors and place at least a 1-µF ceramic capacitor close to the VIN pin. For MLCCs, TI recommends using X7R or X5R dielectrics. Consult capacitor manufacturer datasheet to see how rated capacitance varies over operating conditions.
The output capacitor is selected based upon the desired reduction in LED current ripple. A 1-µF ceramic capacitor results in very low LED current ripple for most applications. Due to the high switching frequency, the
1-µF capacitor alone (without feed-forward capacitor C4) can filter more than 90% of the inductor current ripple for most applications where the sum of LED dynamic resistance and R1 is larger than 1 Ω. Because the internal compensation is tailored for small output capacitance with very low ESR, TI strongly recommends using a ceramic capacitor with capacitance less than 3.3 µF.
Given the availability and quality of MLCCs and the expected output voltage of designs using the LM3405, there is really no need to review other capacitor technologies. A benefit of ceramic capacitors is their ability to bypass high frequency noise. A certain amount of switching edge noise couples through the parasitic capacitances in the inductor to the output. A ceramic capacitor bypasses this noise. In cases where large capacitance is required, use Electrolytic or Tantalum capacitors with large ESR, and verify the loop performance on the bench. Like the input capacitor, multilayer ceramic capacitors are recommended X7R or X5R. Again, verify actual capacitance at the desired operating voltage and temperature.
Check the RMS current rating of the capacitor. The maximum RMS current rating of the capacitor is calculated with Equation 19.
One may select a 1206 size ceramic capacitor for C2, because its current rating is typically higher than 1 A, more than enough for the requirement.
The feed-forward capacitor (designated as C4) connected in parallel with the LED string is required to provide multiple benefits to the LED driver design. It greatly improves the large signal transient response and suppresses LED current overshoot that may otherwise occur during PWM dimming; it also helps to shape the rise and fall times of the LED current pulse during PWM dimming thus reducing EMI emission; it reduces LED current ripple by bypassing some of inductor ripple from flowing through the LED. For most applications, a 1-µF ceramic capacitor is sufficient. In fact, the combination of a 1-µF feed-forward ceramic capacitor and a 1-µF output ceramic capacitor leads to less than 1% current ripple flowing through the LED. Lower and higher C4 values can be used, but bench validation is required to ensure the performance meets the application requirement.
Figure 21 shows a typical LED current waveform during PWM dimming without feed-forward capacitor. At the beginning of each PWM cycle, overshoot can be seen in the LED current. Adding a 1-µF feed-forward capacitor can totally remove the overshoot as shown in Figure 22.
The catch diode (D1) conducts during the switch off-time. A Schottky diode is required for its fast switching time and low forward voltage drop. The catch diode must be chosen such that its current rating is greater than Equation 20.
The reverse breakdown rating of the diode must be at least the maximum input voltage plus appropriate margin. To improve efficiency, choose a Schottky diode with a low forward voltage drop.
TI recommends a standard diode such as the 1N4148 type. For VBOOST circuits derived from voltages less than 3.3 V, a small-signal Schottky diode is recommended for better efficiency. A good choice is the BAT54 small signal diode.
A 0.01-µF ceramic capacitor with a voltage rating of at least 6.3 V is sufficient. The X7R and X5R MLCCs provide the best performance.
The main power loss in LM3405 includes three basic types of loss in the internal power switch: conduction loss, switching loss, and gate charge loss. In addition, there is loss associated with the power required for the internal circuitry of IC.
The conduction loss is calculated with Equation 21.
If the inductor ripple current is fairly small (for example, less than 40%), the conduction loss can be simplified with Equation 22.
The switching loss occurs during the switch on and off transition periods, where voltage and current overlap resulting in power loss. The simplest means to determine this loss is to empirically measure the rise and fall times (10% to 90%) of the voltage at the switch pin.
Switching power loss is calculated with Equation 23.
The gate charge loss is associated with the gate charge QG required to drive the switch with Equation 24.
The power loss required for operation of the internal circuitry is calculated with Equation 25.
IQ is the quiescent operating current, and is typically around 1.8mA for the LM3405.
The total power loss in the IC is Equation 26.
An example of power losses for a typical application is shown in Table 2, Equation 27, and Equation 28 (D is calculated to be 0.36).
CONDITIONS | POWER LOSS | ||
---|---|---|---|
VIN | 12 V | — | — |
VOUT | 3.9 V | — | — |
IOUT | 1 A | — | — |
VD1 | 0.45 V | — | — |
RDS(ON) | 300 mΩ | PCOND | 111 mW |
fSW | 1.6 MHz | — | — |
TRISE | 18 ns | PSW | 288 mW |
TFALL | 12 ns | ||
IQ | 1.8 mA | PQ | 22 mW |
QG | 1.4 nC | PG | 27 mW |
The following are the parameter specifications for this design example:
Calculate the nominal duty cycle for calculations and ensure the maximum duty cycle is not exceeded in the application using Equation 29.
Using the same equation DMAX can be calculated for the minimum input voltage of 4.5 V. The duty cycle at 4.5 V is 0.8 which is less than the minimum DMAX of 0.85 specified in Electrical Characteristics.
Low input voltage applications and PWM dimming applications generally require more input capacitance so the higher value of C1 = 10 µF is chosen for best performance. The other capacitor values chosen are the recommended values of C2 = C4 = 1 µF and C3 = 0.01 µF. All capacitors chosen are X5R or X7R dielectric ceramic capacitors of sufficient voltage rating.
The nominal LED current at 100% PWM dimming duty cycle is set by the resistor R1. R1 can be calculated using Equation 30.
The standard value of R1 = 0.2 Ω is chosen. R1 must have a power rating of at least 1/4 W.
For the boost diode, D2, choose a low current diode with a voltage rating greater than the input voltage to give some margin. D2 must also be a schottky to minimize the forward voltage drop. For this example a schottky diode of D2 = 100 mA, 30 V is chosen. The catch diode, D1, must be a schottky diode and must have a voltage rating greater than the input voltage and a current rating greater than the average current. The average current in D1 can be calculated with Equation 31.
For this example D1 = 1 A, 10 V is chosen.
The inductor value is chosen for a given ripple ratio (r). To calculate L1 the forward voltage of D1 is required. In this case the chosen diode has a forward voltage drop of VF = 0.37 V. Given the desired ripple ratio L1 is calculated with Equation 32.
The next larger standard value of L1 = 4.7 µH is chosen. A ripple ratio of 0.6 translates to a ΔiL of 600 mA and a peak inductor current of 1.3 A (IF + ΔiL/2). Choose an inductor with a saturation current rating of greater than
1.3 A.
PART ID | PART VALUE | PART NUMBER | MANUFACTURER |
---|---|---|---|
U1 | 1-A LED Driver | LM3405 | Texas Instruments |
C1, Input capacitor | 10 µF, 6.3 V, X5R | C3216X5R0J106M | TDK |
C2, Output capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
C3, Boost capacitor | 0.01 µF, 16 V, X7R | 0805YC103KAT2A | AVX |
C4, Feedforward capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
D1, Catch diode | Schottky, 0.37 V at 1A, VR = 10 V | MBRM110LT1G | ON Semiconductor |
D2, Boost diode | Schottky, 0.36 V at 15 mA | CMDSH-3 | Central Semiconductor |
L1 | 4.7 µH, 1.6 A | SLF6028T-4R7M1R6 | TDK |
R1 | 0.2 Ω, 0.5 W, 1% | WSL2010R2000FEA | Vishay |
PART ID | PART VALUE | PART NUMBER | MANUFACTURER |
---|---|---|---|
U1 | 1-A LED Driver | LM3405 | Texas Instruments |
C1, Input capacitor | 10 µF, 25 V, X5R | ECJ-3YB1E106K | Panasonic |
C2, Output capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
C3, Boost capacitor | 0.01 µF, 16 V, X7R | 0805YC103KAT2A | AVX |
C4, Feedforward capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
D1, Catch diode | Schottky, 0.5 V at 1 A, VR = 30 V | SS13 | Vishay |
D2, Boost diode | Schottky, 0.36 V at 15 mA | CMDSH-3 | Central Semiconductor |
L1 | 4.7 µH, 1.6 A | SLF6028T-4R7M1R6 | TDK |
R1 | 0.2 Ω, 0.5 W, 1% | WSL2010R2000FEA | Vishay |
PART ID | PART VALUE | PART NUMBER | MANUFACTURER |
---|---|---|---|
U1 | 1-A LED Driver | LM3405 | Texas Instruments |
C1, Input capacitor | 10 µF, 25 V, X5R | ECJ-3YB1E106K | Panasonic |
C2, Output capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
C3, Boost capacitor | 0.01 µF, 16 V, X7R | 0805YC103KAT2A | AVX |
C4, Feedforward capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
D1, Catch diode | Schottky, 0.5 V at 1A, VR = 30 V | SS13 | Vishay |
D2, Boost diode | Schottky, 0.36 V at 15 mA | CMDSH-3 | Central Semiconductor |
D3, Zener diode | 11 V, 350 mW, SOT-23 | BZX84C11 | Fairchild |
L1 | 6.8 µH, 1.5 A | SLF6028T-6R8M1R5 | TDK |
R1 | 0.2 Ω, 0.5 W, 1% | WSL2010R2000FEA | Vishay |
PART ID | PART VALUE | PART NUMBER | MANUFACTURER |
---|---|---|---|
U1 | 1-A LED Driver | LM3405 | Texas Instruments |
C1, Input capacitor | 10 µF, 25 V, X5R | ECJ-3YB1E106K | Panasonic |
C2, Output capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
C3, Boost capacitor | 0.01 µF, 16 V, X7R | 0805YC103KAT2A | AVX |
C4, Feedforward capacitor | 1 µF, 10 V, X7R | GRM319R71A105KC01D | Murata |
C5, Shunt capacitor | 0.1 µF, 16 V, X7R | GRM219R71C104KA01D | Murata |
D1, Catch diode | Schottky, 0.5 V at 1 A, VR = 30 V | SS13 | Vishay |
D2, Boost diode | Schottky, 0.36 V at 15 mA | CMDSH-3 | Central Semiconductor |
D3, Zener diode | 4.7 V, 350 mW, SOT-23 | BZX84C4 V7 | Fairchild |
L1 | 6.8 µH, 1.5 A | SLF6028T-6R8M1R5 | TDK |
R1 | 0.2 Ω, 0.5 W, 1% | WSL2010R2000FEA | Vishay |
R2 | 1.91 kΩ, 1% | CRCW08051K91FKEA | Vishay |
PART ID | PART VALUE | PART NUMBER | MANUFACTURER |
---|---|---|---|
U1 | 1-A LED Driver | LM3405 | Texas Instruments |
C1, Input capacitor | 10 µF, 25 V, X5R | ECJ-3YB1E106K | Panasonic |
C2, Output capacitor | 1 µF, 16 V, X7R | GRM319R71A105KC01D | Murata |
C3, Boost capacitor | 0.01 µF, 16 V, X7R | 0805YC103KAT2A | AVX |
C4, Feedforward capacitor | 1 µF, 16 V, X7R | GRM319R71A105KC01D | Murata |
D1, Catch diode | Schottky, 0.5 V at 1 A, VR = 30 V | SS13 | Vishay |
D2, Boost diode | Schottky, 0.36 V at 15 mA | CMDSH-3 | Central Semiconductor |
D3, Zener diode | 11 V, 350 mW, SOT-23 | BZX84C11 | Fairchild |
L1 | 6.8 µH, 1.5 A | SLF6028T-6R8M1R5 | TDK |
R1 | 0.2 Ω, 0.5 W, 1% | WSL2010R2000FEA | Vishay |