JAJSS26 March 2011 – November 2023 LM3481-Q1
PRODUCTION DATA
The most common topology for the LM3481-Q1 is the boost or step-up topology. The boost converter converts a low input voltage into a higher output voltage. The basic configuration for a boost regulator is shown in Figure 7-2. In continuous conduction mode (when the inductor current never reaches zero at steady state), the boost regulator operates in two cycles. In the first cycle of operation, MOSFET Q is turned on and energy is stored in the inductor. During this cycle, diode D1 is reverse biased and load current is supplied by the output capacitor, COUT.
In the second cycle, MOSFET Q is off and the diode is forward biased. The energy stored in the inductor is transferred to the load and output capacitor. The ratio of these two cycles determines the output voltage. The output voltage is defined as:
(ignoring the voltage drop across the MOSFET and the diode), or
where D is the duty cycle of the switch, VD1 is the forward voltage drop of the diode, and VQ is the drop across the MOSFET when it is on. The following sections describe selection of components for a boost converter.