SNVSCV4 September 2024 LM3645
PRODUCTION DATA
In order for current to flow in the LEDs, the appropriate Dx_EN bits in Configuration Register 2 must be set to logic '1' (bits [3:0) in reg 0x01). When enabled, the Dx outputs will behave based upon the mode that pin is set to (DMODE register). If the Dx_EN bit is set to a '0', the output will remain off regardless of the mode the output is placed in. At the end of an I2C controlled flash event when a time-out occurs, the Dx_EN bits will auto-clear. If the mode is changed during an I2C controlled flash, the Dx_EN bit will not autoclear. When used along with the strobe pins, the Dx_EN pins do not automatically reset unless a fault event occurs.