JAJSJK6D October 2007 – August 2020 LM5067
PRODUCTION DATA
The current limit threshold is reached when the voltage across the sense resistor RS (SENSE to VEE) reaches 50 mV. In the current limiting condition, the GATE voltage is controlled to limit the current in MOSFET Q1. While the current limit circuit is active, the fault timer is active as described in the Section 8.3.6 section. If the load current reduces below the current limit threshold before the end of the Fault Timeout Period, the LM5067 resumes normal operation. For proper operation, the RS resistor value should be no larger than 100 mΩ.