JAJSRS8I February 2007 – November 2023 LM5116
PRODUCTION DATA
A voltage divider and filter can be connected to the UVLO pin to set a minimum operating voltage VIN(MIN) for the regulator. If this feature is required, the following procedure can be used to determine appropriate resistor values for RUV2, RUV1 and CFT.
If undervoltage shutdown is not required, RUV1 and RUV2 can be eliminated and the off-time becomes:
The voltage at the UVLO pin must never exceed 16 V when using an external set-point divider. It can be necessary to clamp the UVLO pin at high input voltages. For the design example, RUV2 = 102 kΩ and RUV1 = 21 kΩ for a shut-down voltage of 6.6 V. If sustained short circuit protection is required, CFT ≥ 1 µF will limit the short circuit power dissipation. D2 can be installed when using CFT with RUV1 and RUV2.