SLVSES8A October 2020 – December 2020 LM5127-Q1
PRODUCTION DATA
For applications requiring the lowest cost with minimum conduction loss, inductor DC resistance (DCR) can be used to sense the inductor current rather than using a sense resistor. RDCRC and CDCRC must meet Equation 23 to match the time constant.
When CH1 is used as a pre-boost, the output undershoot during a cold-cranking event can be minimized by adding an R-C in parallel with the low-side feedback resistor. A lower value of ROS will result in a lower output undershoot (see Figure 9-3). The COS value should be large enough not to affect loop response in normal operation. Use 20-kΩ and 4.7-nF combination as a starting point and then adjust the values if required.
The light load switching mode can be dynamically programmed during operation between FPWM and DE mode.
If required, an additional PGOOD or BMOUT delay can be programmed using an external circuit.
Sequential start-up can be realized by using the PGOOD pins.
Switching can be stopped individually by pulling down the SS pins.