JAJSUV0 June 2024 LM5171
PRODUCTION DATA
TI recommends setting a hard limit of the maximum current programming signal such that the converter cannot be over driven by an errant current programming signal. Assume the converter is allowed up to 10% overloading current. Refer to Channel Current Setting Commands (ISET1 and ISET2), the analog current setting signal ISETx must be limited by the following voltage level:
As shown in Figure 7-6, RISETT and RISETB are used to limit the maximum voltage on ISETx.