JAJSUV0 June 2024 LM5171
PRODUCTION DATA
For best current monitor accuracy, choose IMONx resistor that the maximum operating voltage on the IMONx pin is less than 3V.
Considering two phase current monitoring with maximum 50A for each channel, and make sure IMONx voltage no more than 3V, RIMONx can be find as:
Choose CIMONx considering delay and voltage ripple. Here we select:
Then the delay of the monitor is determined by the following time constant:
At full load, the DC component of the monitor voltage is:
Considering the inductor ripple current, according to Equation 6, the IOUT peak to peak ripple current is:
The RC filter corner frequency is thus given by:
The resulting peak-to-peak monitor ripple voltage is approximately determined by:
The peak-to-peak monitor ripple voltage is approximately 0.34% of the full load DC monitor voltage. Increasing CIMONx attenuates the ripple voltage at the cost of higher monitor delay.