JAJSOR1D june 2022 – august 2023 LM5177
PRODUCTION DATA
Figure 8-23 describes the functional behavior of the internal device logic.
DEVICE_OFF
During the DEVICE_OFF state the LM5177 is in shutdown. All internal logic and the DC/DC converter as well as the gate driver are off. The internal POR- system monitors the EN threshold to start the initialization of the reference system an device logic. The device current consumption is given by the shutdown current.
MAIN_LOGIC_ON
Once the LM5177 transits to the MAIN_LOGIC_ON state it will first stay in the POWER_STAGE_OFF state. Here the necessary checks and preparation for the start up are taken. The current consumption is given by the standby current.
HOLD-R2D
In this state the CFG-pin settings are read and the logic is storing this settings until the next EN -pin cycle.
READ_R2D
During the READ-R2D state the LM5177 executives the reading of the CFG-pin to get the selected settings determined by placed resistor.
POWER_STAGE_ACTIVE
The device executes the soft-start ramp during each entry to this state to avoid excessive inrush currents. In this state the power stage is active and the converter in operation. The current consumption is given by the active quiescent current of the electrical specification table.
TSD
The device enters the TSD-state if the silicon junction temperature exceeds the thermal shutdown limit. It automatically transits back to the POWER_STAGE_ACTIVE -state once the hysteresis of the thermal shutdown triggers.