JAJSOR1D june 2022 – august 2023 LM5177
PRODUCTION DATA
Pin | Type(1) | Description | |
---|---|---|---|
Name | No. | ||
AGND | 17 | G | Analog ground of the device |
BIAS | 1 | I | Optional input to the VCC bias regulator. Powering VCC from an external supply instead of VIN can reduce power loss at high VIN. If the bias pin supply is not used in the application connect the pin GND |
CFG | 13 | I/O | Device configuration pin. Connect a resistor between the CFG pin to select the device operation for spread spectrum (DRSS), short circuit protection (hiccup mode), current limit, or current monitor. |
COMP | 18 | O | Output of the error amplifier. An external RC network connected between COMP and AGND compensates the regulator of the output voltage feedback loop. |
CSA | 37 | I | Inductor peak current sensor positive input. Connect CSA to the positive side of the external current sense resistor using a low-current Kelvin connection. |
CSB | 38 | I | Inductor peak current sense negative input. Connect CSB to the negative side of the external current sense resistor using a low-current Kelvin connection. |
DTRK | 10 | I | Digital PWM input pin for the dynamical output voltage tracking. Do not leave this pin floating. If this function is not used, connect the pin to VCC or GND. |
EN/UVLO | 4 | I | Enable pin. The pin enables or disables the device. If the pin is less than 0.6 V, the device shuts down. The pin must be raised above 0.65 V to enable the device. This pin is the enable pin for the device internal reference circuit and input voltage UVLO comparator input. |
FB | 19 | I | Feedback pin for output voltage regulation. Connect a resistor divider network from the output of the converter to the FB pin. |
HB1 | 35 | P | Bootstrap supply pin for buck half-bridge. An external capacitor is required between the HB1 pin and the SW1 pin, respectively, to provide bias to the high-side MOSFET gate driver. |
HO1 | 34 | O | High-side gate driver output for the buck half-bridge |
HO1_LL | 8 | O | Logic level output of the HO1 gate signal. Connect this ground reference PWM signal to an optional external gate-driver input. If the function is not used, make no external connection to this pin. |
HB2 | 26 | P | Bootstrap supply pin for boost half-bridge. An external capacitor is required between the HB2 pin and the SW2 pin, respectively, to provide bias to the high-side MOSFET gate driver. |
HO2 | 27 | O | High-side gate driver output for the boost half-bridge |
HO2_LL | 9 | O | Logic level output of the HO2 gate signal. Connect this ground reference PWM signal to an optional external gate-driver input. If the function is not used, make no external connection to this pin. |
IMONOUT | 6 | O | Current monitor output pin. Output of the voltage-controlled current source of the optional current monitor. Connect the pin to a resistor to sense the voltage across. If the output or input current sense amplifier is configured as current limiter, an external RC network connected between IMONOUT and AGND compensates the regulator of the current feedback loop. Connect the IMONOUT pin to VCC to disable the block and reduce the quiescent current |
ISNSN | 22 | I | Negative sense input of the output or input current sense amplifier. An optional current sense resistor connected between ISNSN and ISNSP can be located either on the input side or on the output side of the power stage. In case the current monitor is disabled connect ISNSN to ground |
ISNSP | 23 | I | Positive sense input of the output or input current sense amplifier. An optional current sense resistor connected between ISNSN and ISNSP can be located either on the input side or on the output side of the power stage. In case the current monitor is disabled connect ISNSN to ground |
LO1 | 32 | O | Low-side gate driver output for the buck half-bridge |
LO2 | 29 | O | Low-side gate driver output for the boost half-bridge |
MODE | 12 | I | Digital input to select device operation mode. If the pin is pulled low, power save mode (PSM) is enabled. If the pin is pulled high, the forced PWM or CCM operation is enabled. The configuration can be changed dynamically during operation. Do not leave this pin floating. If this function is not used, connect the pin to VCC or GND. |
NC | 2 | NC | No internal connection |
NC | 5 | NC | No internal connection |
NC | 21 | NC | No internal connection |
NC | 24 | NC | No internal connection |
NC | 28 | NC | No internal connection |
NC | 33 | NC | No internal connection |
nFLT | 7 | O | Open-drain output pin for fault indication or power good. This pin is pulled low when FB is outside a ±10% regulation window around the regulation window of the nominal output voltage. If the nFLT pin function is not used the pin can be kept floating. |
PowerPAD | PAD | G | Connect the PowerPAD to the analog ground. Use thermal vias to connect to a PCB ground plane for improved power dissipation. |
PGND | 30 | G | Power ground. This pin is the high current ground connection to the low-side gate drivers and for the internal VCC regulator. |
RT | 15 | I/O | Switching frequency programming pin. An external resistor is connected to the RT pin and AGND to set the switching frequency. |
SLOPE | 14 | I | A resistor connected between the SLOPE pin and AGND provides the slope compensation ramp for stable current mode operation in both buck and boost mode. |
SS/ATRK | 16 | I/O | Soft-start programming pin. A capacitor between the SS pin and AGND pin programs soft-start time. Analog output voltage tracking pin. The VOUT regulation target can be programmed by connecting the pin to variable voltage reference (for example, through a digital to analog converter). The internal circuit selects the lowest voltage applied to the pin. |
SW1 | 36 | P | Inductor switch node for the buck half-bridge |
SW2 | 25 | P | Inductor switch node for the boost half-bridge |
SYNC | 11 | I | Synchronization clock input. The internal oscillator can be synchronized to an external clock during operation. If the output or input current sense amplifier is configured as a current limiter pulling, this pin is low during start-up, device switches the current limit direction to a negative polarity. Do not leave this pin floating. If this function is not used, connect the pin to VCC. |
VCC | 31 | P | Internal linear bias regulator output. Connect a ceramic decoupling capacitor from VCC to PGND. |
VIN | 3 | I | The input supply and sense input of the device. Connect VIN to the supply voltage of the power stage. |
VOUT | 20 | I | VOUT sense input. Connect to the power stage output rail. |