JAJS854E May 1999 – December 2024 LM6172
PRODUCTION DATA
The combination of an amplifier input capacitance with gain-setting resistors adds a pole that can cause peaking or oscillation. To solve this problem, a feedback capacitor with the following value can be used to cancel that pole:
For the LM6172, a feedback capacitor of 2pF is recommended. Figure 7-4 illustrates the compensation circuit.