JAJSKN8 September 2021 LM74700-EP
PRODUCTION DATA
PIN | I/O(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | EN | I | Enable pin. Can be connected to ANODE for always ON operation. |
2 | GND | G | Ground pin |
3 | N.C | No connection. Keep this pin floating. | |
4 | VCAP | O | Charge pump output. Connect to external charge pump capacitor. |
5 | ANODE | I | Anode of the diode and input power. Connect to the source of the external N-channel MOSFET. |
6 | GATE | O | Gate drive output. Connect to gate of the external N-channel MOSFET. |
7 | N.C | No connection. Keep this pin floating. | |
8 | CATHODE | I | Cathode of the diode. Connect to the drain of the external N-channel MOSFET. |