JAJSI47B April 2017 – October 2019 LMH0397
PRODUCTION DATA.
The LMH0397 supports SPI daisy-chaining among multiple devices, as shown in Figure 19.
Each LMH0397 device is directly connected to the SCK and SS_N pins of the host. The first LMH0397 device in the chain is connected to the MOSI pin of the host, and the last device in the chain is connected to the MISO pin of the host. The MOSI pin of each intermediate LMH0397 device in the chain is connected to the MISO pin of the previous LMH0397 device, thereby creating a serial shift register. In a daisy-chain configuration of N × LMH0397 devices, the host conceptually sees a shift register of length 17 × N for a basic SPI transaction, during which SS_N is asserted low for 17 × N clock cycles.