JAJSFM3E February 2015 – June 2018 LMH1218
PRODUCTION DATA.
The following example make some assumptions:
The daisy-chain is 3 LMH1218 devices long, comprising Devices 1, 2, and 3 as shown in Figure 18. Therefore, each Basic SPI Transaction is 17x3 = 51 clocks long.
In Figure 19, the following occurs at the end of the transaction:
Note that the bits are shifted out of MOSI left to right. The MISO pin is not shown as it reflects shift register contents from a prior transaction.