JAJSI48C March 2017 – October 2019 LMH1228
PRODUCTION DATA.
The LOCK_N pin can be reconfigured through register control to indicate a SD_N (signal detect) event. When configured as a SD_N output, the pin asserts low at the end of adaptation after a valid signal is detected by the IN0 signal detect circuit. For more information about how to configure the LOCK_N pin for SD_N functionality, refer to the LMH1228 and LMH1208 Programming Guide (SNAU206).