JAJSJA6A September 2021 – December 2021 LMH5485-SP
ADVANCE INFORMATION
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
The design equations for setting the resistors around an FDA to convert from a single-ended input signal to differential output can be approached from several directions. Here, several critical assumptions are made to simplify the results:
Both of these assumptions are typical and aimed to delivering the best dynamic range through the FDA signal path.
Figure 8-1 and Figure 8-3 shows how after the feedback resistor values are chosen, the aim is to solve for the Rt (a termination resistor to ground on the signal input side), Rg1 (the input gain resistor for the signal path), and Rg2 (the matching gain resistor on the nonsignal input side). The same resistor solutions can be applied to either AC- or DC-coupled paths. Adding blocking capacitors in the input-signal chain is a simple option. Figure 8-1 shows how adding these blocking capacitors after the Rt element has the advantage of removing any DC currents in the feedback path from the output Vocm to ground.
Earlier approaches to the solutions for Rt and Rg1 (when the input must be matched to a source impedance, Rs) follow an iterative approach. This complexity arises from the active input impedance at the Rg1 input. When the FDA is used to convert a single-ended signal to differential, the common-mode input voltage at the FDA inputs must move with the input signal to generate the inverted output signal as a current in the Rg2 element. Equation 1shows a more recent solution, where a quadratic in Rt can be solved for an exact required value. This quadratic emerges from the simultaneous solution for a matched input impedance and target gain. The only inputs required are the following:
As Equation 1 shows, solving this quadratic for Rt starts the solution sequence.
Being a quadratic, there are limits to the range of solutions. Specifically, after Rf and Rs are chosen, there is physically a maximum gain beyond which Equation 1 starts to solve for negative Rt values (if input matching is a requirement). With Rf selected, use Equation 2 to verify that the maximum gain is greater than the desired gain.
If the achievable Avmax is less than desired, increase the Rf value. After Rt is derived from Equation 1, the Rg1 element is given by Equation 3:
Then, the simplest approach is to use a single Rg2 = Rt || Rs + Rg1 on the nonsignal input side. Often, this approach is shown as the separate Rg1 and Rs elements. Using these separate elements provide a better divider match on the two feedback paths, but a single Rg2 is often acceptable. A direct solution for Rg2 is given as Equation 4:
This design proceeds from a target input impedance matched to Rs, signal gain Av from the matched input to the differential output voltage, and a selected Rf value. The nominal Rf value chosen for the LMH5485-SP characterization is 402 Ω. As discussed previously, going lower improves noise and phase margin, but reduces the total output load impedance possibly degrading harmonic distortion. Going higher increases the output noise, and might reduce the loop-phase margin because of the feedback pole to the input capacitance, but reduces the total loading on the outputs. Using Equation 2 to Equation 4 to sweep the target gain from 1 to Avmax < 14.3 V/V gives Table 9-1, which shows exact values for Rt, Rg1, and Rg2, where a 50 Ω source must be matched while setting the two feedback resistors to 402 Ω. One possible solution for 1% standard values is shown along with the resulting actual input impedance and gain with % errors to the targets in Table 9-1.
Av(1) | Rt, EXACT (Ω) | Rt 1% | Rg1, EXACT (Ω) | Rg1 1% | Rg2, EXACT (Ω) | Rg2 1% | ACTUAL ZIN | %ERR TO Rs | ACTUAL GAIN | %ERR TO Av |
---|---|---|---|---|---|---|---|---|---|---|
1 | 55.2 | 54.9 | 395 | 392 | 421 | 422 | 49.731 | –0.54% | 1.006 | 0.62% |
2 | 60.1 | 60.4 | 193 | 191 | 220 | 221 | 50.171 | 0.34% | 2.014 | 0.72% |
3 | 65.6 | 64.9 | 123 | 124 | 151 | 150 | 49.572 | –0.86% | 2.983 | –0.57% |
4 | 72.0 | 71.5 | 88.9 | 88.7 | 118 | 118 | 49.704 | –0.59% | 4.005 | 0.14% |
5 | 79.7 | 80.6 | 68.4 | 68.1 | 99.2 | 100 | 50.451 | 0.90% | 5.014 | 0.28% |
6 | 89.1 | 88.7 | 53.7 | 53.6 | 85.7 | 86.6 | 49.909 | –0.18% | 6.008 | 0.14% |
7 | 101 | 102 | 43.5 | 43.2 | 77.1 | 76.8 | 50.179 | 0.36% | 7.029 | 0.42% |
8 | 117 | 118 | 35.5 | 35.7 | 70.6 | 69.8 | 50.246 | 0.49% | 7.974 | –0.32% |
9 | 138 | 137 | 28.8 | 28.7 | 65.4 | 64.9 | 49.605 | –0.79% | 9.016 | 0.18% |
10 | 170 | 169 | 23.5 | 23.7 | 62.0 | 61.9 | 50.009 | 0.02% | 9.961 | –0.39% |
11 | 220 | 221 | 18.8 | 18.7 | 59.6 | 59.0 | 49.815 | –0.37% | 11.024 | 0.22% |
12 | 313 | 316 | 14.7 | 14.7 | 57.9 | 57.6 | 50.051 | 0.10% | 11.995 | –0.04% |
13 | 545 | 549 | 10.9 | 11.0 | 56.7 | 56.2 | 49.926 | –0.15% | 12.967 | –0.25% |
14 | 2209 | 2210 | 7.26 | 7.32 | 56.2 | 56.2 | 50.079 | 0.16% | 13.986 | –0.10% |
These equations and design flow apply to any FDA. Using the feedback resistor value as a starting point is particularly useful for current-feedback-based FDAs such as the LMH6554, where the value of these feedback resistors determines the frequency response flatness. Similar tables can be built using the equations provided here for other source impedances, Rf values, and gain ranges.
Note the extremely low Rg1 values at the higher gains. For instance, at a gain of 14 V/V, that 7.32 Ω standard value is transformed by the action of the common-mode loop moving the input common-mode voltage to appear like a 50 Ω input match. This active input impedance provides an improved input-referred noise at higher gains. The TINA model correctly shows this actively-set input impedance in the single-ended to differential configuration, and is a good tool to validate the gains, input impedances, response shapes, and noise issues.