SNAS674B September 2015 – February 2017 LMK61E2
PRODUCTION DATA.
The LMK61E2 is a programmable oscillator that generates commonly used reference clocks with less than 200-fs RMS maximum random jitter in integer PLL mode and less than 300-fs RMS maximum random jitter in fractional PLL mode.
NOTE
Control blocks are compatible with 1.8, 2.5, or 3.3-V I/O voltage levels.
The LMK61E2 comprises of an integrated oscillator that includes a 50-MHz crystal, a fractional PLL with integrated VCO that supports a frequency range of 4.6 GHz to 5.6 GHz. The PLL block consists of a phase frequency detector (PFD), charge pump, integrated passive loop filter, a feedback divider that can support both integer and fractional values and a delta-sigma engine for noise suppression in fractional PLL mode. Completing the device is the combination of an integer output divider and a universal differential output buffer. The PLL is powered by on-chip low dropout (LDO) linear voltage regulators and the regulated supply network is partitioned such that the sensitive analog supplies are running from separate LDOs than the digital supplies which use their own LDO. The LDOs provide isolation to the PLL from any noise in the external power supply rail with a PSRR of better than –70 dBc at 50-kHz to 1-MHz ripple frequencies at 3.3-V device supply. The device supports fine and coarse frequency margining by changing the settings of the integrated oscillator and the output divider respectively.
The LMK61E2 supports I2C programming interface where an I2C host can update any device configuration after the device enables the host interface and the host writes a sequence that updates the device registers. Once the device configuration is set, the host can also write to the on-chip EEPROM for a new set of power-up defaults based on the configuration pin settings in the soft pin configuration mode.
Figure 24 shows the method that this document employs to refer to an individual register bit or a grouping of register bits. If a drawing or text references an individual bit the format is to specify the register number first and the bit number second. The LMK61E2 contains 38 registers that are 8 bits wide. The register addresses and the bit positions both begin with the number zero (0). A period separates the register address and bit address. The first bit in the register file is address ‘R0.0’ meaning that it is located in Register 0 and is bit position 0. The last bit in the register file is address ‘R72.7’ referring to the 8th bit of register address 72 (the 73rd register in the device). Figure 24 also lists specific bit positions as a number contained within a box. A box with the register address encloses the group of boxes that represent the bits relevant to the specific device circuitry in context.
The PLL in LMK61E2 can be configured to accommodate various output frequencies either through I2C programming interface or in the absence of programming, the PLL defaults stored in EEPROM is loaded on power up. The PLL can be configured by setting the Reference Doubler, Integrated PLL Loop Filter, Feedback Divider, and Output Divider.
For the PLL to operate in closed-loop mode, the following condition in Equation 1 has to be met.
where
The output frequency is related to the VCO frequency as given in Equation 2.
where
The integrated oscillator in LMK61E2 features programmable load capacitances that can be set to either operate at exactly its nominal oscillation frequency or operate at a fixed frequency offset from its nominal oscillation frequency. This is done by programming R16 and R17. More details on frequency margining are provided in Fine Frequency Margining.
The reference path has a frequency doubler that can be enabled by programming R34.5 = 1. Enabling the doubler allows a higher comparison frequency for the PLL and would result in a 3-dB reduction in the in-band phase noise at the output of the LMK61E2. Enabling the doubler also results in higher reference and phase detector spurs which will be minimized by enabling the higher order components (R3, C3) of the loop filter and programmed to appropriate values. Disabling the doubler would result in higher in-band phase noise on the device output than when the doubler is enabled but the reference and phase detector spurs would be lower on the device output than when the doubler is enabled.
The Phase Frequency Detector (PFD) of the PLL takes inputs from the reference path and the feedback divider output and produces an output that is dependent on the phase and frequency difference between the two inputs. The input frequency of the PFD is 50 MHz when reference doubler is disabled, or 100 MHz when reference doubler is enabled.
The N divider of the PLL includes fractional compensation and can achieve any fractional denominator (DEN) from 1 to 4,194,303. The integer portion, INT, is the whole part of the N divider value and the fractional portion, NUM / DEN, is the remaining fraction. INT, NUM, and DEN are programmed in R25, R26, R27, R28, R29, R30, R31, and R32. The total programmed N divider value, N, is determined by: N = INT + NUM / DEN. The output of the N divider sets the PFD frequency to the PLL and should equal 50 MHz, when reference doubler is disabled, or 100 MHz, when reference doubler is enabled.
The delta signal modulator is a key component of the fractional circuitry and is involved in noise shaping for better phase noise and spurs in the band of interest. The order of the delta sigma modulator is selectable between integer mode and third order, for fractional PLL mode, and can be programmed in R33[1-0]. Dithering can be programmed in R33[3-2] and should be disabled for integer PLL mode and set to weak for fractional PLL mode.
The PLL has charge pump slices of 1.6 mA, to be used when PLL is set to fractional mode, or 6.4 mA, to be used when PLL is set to integer mode. These slices can be selected by programming R34[3-0]. When PLL is set to fractional mode, a phase shift needs to be introduced to maintain a linear response and ensure consistent performance across operating conditions and a value of 0x2 should be programmed in R35[6-4]. When PLL is set to integer mode, a value of 0x0 should be programmed in R35[6-4].
The LMK61E2 features a fully integrated loop filter for the PLL and supports programmable loop bandwidth from 100 kHz to 1 MHz. The loop filter components, R2, C1, R3, and C3 can be configured by programming R36, R37, R38, and R39 respectively. The LMK61E2 features a fixed value of C2 of 10 nF. When PLL is configured in the fractional mode, R35.2 should be set to 1. When reference doubler is disabled for integer mode PLL, R35.2 should be set to 0 and R38[6-0] should be set to 0x00. When reference doubler is enabled for integer mode PLL, R35.2 should be set to 1 and R38 and R39 are written with the appropriate values. Figure 25 shows the loop filter structure of the PLL. It is important to set the PLL to best possible bandwidth to minimize output jitter. TI provides the WEBENCH® Clock Architect Tool that makes it easy to select the right loop filter components.
The PLL in LMK61E2 is made of LC VCO that is designed using high-Q monolithic inductors to oscillate between 4.6 GHz and 5.6 GHz and has low-phase noise characteristics. The VCO must be calibrated to ensure that the clock outputs deliver optimal phase noise performance. Fundamentally, a VCO calibration establishes an optimal operating point within the tuning range of the VCO. Setting R72.1 to 1 causes a VCO recalibration and is necessary after device reconfiguration. VCO calibration automatically occurs on device power up.
The high-speed output divider supports divide values of 5 to 511 and are programmed in R22 and R23. The output divider also supports coarse frequency margining that can initiate as low as a 5% change in the output frequency.
The clock output can be configured as LVPECL, LVDS, or HCSL by programming R21[1-0]. Interfacing to LVPECL, LVDS, or HCSL receivers are done either with direct coupling or with AC-coupling capacitor as shown in Figure 16 – Figure 21.
The LVDS output structure has integrated 125-Ω termination between each side (P and N) of the differential pair. The HCSL output structure is open drain and can be DC or AC coupled to HCSL receivers with appropriate termination scheme. The LVPECL output structure is an emitter follower requiring external termination.
The PLL loss of lock and PLL calibration status can be monitored by reading R66[1-0]. These bits represent a logic-high interrupt output and are self-cleared once the readback is complete.
The PLL loss of lock detection circuit is a digital circuit that detects any frequency error, even a single cycle slip. Loss of lock may occur when an incorrect PLL configuration is programmed or the VCO has not been recalibrated.
The host (DSP, Microcontroller, FPGA, and so forth) configures and monitors the LMK61E2 through the I2C port. The host reads and writes to a collection of control and status bits called the register map. The device blocks can be controlled and monitored through a specific grouping of bits located within the register file. The host controls and monitors certain device Wide critical parameters directly through register control and status bits. In the absence of the host, the LMK61E2 can be configured to operate from its on-chip EEPROM. The EEPROM array is automatically copied to the device registers upon power up. The user has the flexibility to rewrite the contents of EEPROM from the SRAM up to a 100 times.
Within the device registers, there are certain bits that have read or write access. Other bits are read-only (an attempt to write to a read-only bit does not change the state of the bit). Certain device registers and bits are reserved, meaning that they must not be changed from their default reset state. Figure 26 shows interface and control blocks within LMK61E2 and the arrows refer to read access from and write access to the different embedded memories (EEPROM, SRAM).
The I2C port on the LMK61E2 works as a slave device and supports both the 100-kHz standard mode and 400-kHz fast mode operations. Fast mode imposes a glitch tolerance requirement on the control signals. Therefore, the input receivers ignore pulses of less than 50 ns duration. The I2C timing is given in I2C-Compatible Interface Characteristics (SDA, SCL). The timing diagram is given in Figure 27.
In an I2C bus system, the LMK61E2 acts as a slave device and is connected to the serial bus (data bus SDA and lock bus SCL). These are accessed via a 7-bit slave address transmitted as part of an I2C packet. Only the device with a matching slave address responds to subsequent I2C commands. In soft pin mode, the LMK61E2 allows up to three unique slave devices to occupy the I2C bus based on the pin strapping of ADD (tied to VDD, GND, or left open). The device slave address is 10110xx (the two LSBs are determined by the ADD pin).
During the data transfer through the I2C interface, one clock pulse is generated for each data bit transferred. The data on the SDA line must be stable during the high period of the clock. The high or low state of the data line can change only when the clock signal on the SCL line is low. The start data transfer condition is characterized by a high-to-low transition on the SDA line while SCL is high. The stop data transfer condition is characterized by a low-to-high transition on the SDA line while SCL is high. The start and stop conditions are always initiated by the master. Every byte on the SDA line must be eight bits long. Each byte must be followed by an acknowledge bit and bytes are sent MSB first. The I2C register structure of the LMK61E2 is shown in Figure 28.
The acknowledge bit (A) or non-acknowledge bit (A’) is the 9th bit attached to any 8-bit data byte and is always generated by the receiver to inform the transmitter that the byte has been received (when A = 0) or not (when A’ = 0). A = 0 is done by pulling the SDA line low during the 9th clock pulse and A’ = 0 is done by leaving the SDA line high during the 9th clock pulse.
The I2C master initiates the data transfer by asserting a start condition which initiates a response from all slave devices connected to the serial bus. Based on the 8-bit address byte sent by the master over the SDA line (consisting of the 7-bit slave address (MSB first) and an R/W’ bit), the device whose address corresponds to the transmitted address responds by sending an acknowledge bit. All other devices on the bus remain idle while the selected device waits for data transfer with the master.
After the data transfer has occurred, stop conditions are established. In write mode, the master asserts a stop condition to end data transfer during the 10th clock pulse following the acknowledge bit for the last data byte from the slave. In read mode, the master receives the last data byte from the slave but does not pull SDA low during the 9th clock pulse. This is known as a non-acknowledge bit. By receiving the non-acknowledge bit, the slave knows the data transfer is finished and enters the idle mode. The master then takes the data line low during the low period before the 10th clock pulse, and high during the 10th clock pulse to assert a stop condition. A generic transaction is shown in Figure 29.
The LMK61E2 I2C interface supports Block Register Write/Read, Read/Write SRAM, and Read/Write EEPROM operations. For Block Register Write/Read operations, the I2C master can individually access addressed registers that are made of an 8-bit data byte. The offset of the indexed register is encoded in the register address, as described in Table 1.
DEVICE | A6 | A5 | A4 | A3 | A2 | ADD pin | R/W |
---|---|---|---|---|---|---|---|
LMK61E2 | 1 | 0 | 1 | 1 | 0 | 0x0, 0x1 or 0x3 | 1/0 |
The I2C Block Register Write transaction is illustrated in Figure 30 and consists of the following sequence.
The I2C Block Register Read transaction is illustrated in Figure 31 and consists of the following sequence.
The on-chip SRAM is a volatile, shadow memory array used to temporarily store register data, and is intended only for programming the non-Volatile EEPROM. The SRAM has the identical data format as the EEPROM map. The register configuration data can be transferred to the SRAM array through special memory access registers in the register map. To successfully program the SRAM, the complete base array and at least one page should be written. The following details the programming sequence to transfer the device registers into the SRAM.
The SRAM can also be written with particular values according to the following programming sequence.
NOTE
It is possible to increment SRAM address incorrectly when 2 successive accesses are made to R51.
The on-chip EEPROM is a non-Volatile memory array used to permanently store register data for a custom device start-up configuration setting to initialize registers upon power up or POR. The EEPROM is comprised of bits shown in the EEPROM Map. The transfer must first happen to the SRAM and then to the EEPROM. During EEPROM write, R49.2 is a 1 and the EEPROM contents cannot be accessed. The following details the programming sequence to transfer the entire contents of SRAM to EEPROM.
The contents of the SRAM can be read out, one word at a time, starting with that of the requested address. Following details the programming sequence for an SRAM read by address.
NOTE
It is possible to increment SRAM address incorrectly when 2 successive accesses are made to R51.
The contents of the EEPROM can be read out, one word at a time, starting with that of the requested address. Following details the programming sequence for an EEPROM read by address.
NOTE
It is possible to increment EEPROM address incorrectly when 2 successive accesses are made to R51.
Any bit that is labeled as RESERVED should be written with a 0.
Byte # | Bit7 | Bit6 | Bit5 | Bit4 | Bit3 | Bit2 | Bit1 | Bit0 |
---|---|---|---|---|---|---|---|---|
0 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
1 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
2 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
3 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
4 | NVMSCRC[7] | NVMSCRC[6] | NVMSCRC[5] | NVMSCRC[4] | NVMSCRC[3] | NVMSCRC[2] | NVMSCRC[1] | NVMSCRC[0] |
5 | NVMCNT[7] | NVMCNT[6] | NVMCNT[5] | NVMCNT[4] | NVMCNT[3] | NVMCNT[2] | NVMCNT[1] | NVMCNT[0] |
6 | 1 | RESERVED | RESERVED | RESERVED | RESERVED | 1 | RESERVED | RESERVED |
7 | RESERVED | RESERVED | 1 | RESERVED | RESERVED | RESERVED | RESERVED | 1 |
8 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
9 | SLAVEADR[7] | SLAVEADR[6] | SLAVEADR[5] | SLAVEADR[4] | SLAVEADR[3] | RESERVED | RESERVED | RESERVED |
10 | EEREV[7] | EEREV[6] | EEREV[5] | EEREV[4] | EEREV[3] | EEREV[2] | EEREV[1] | EEREV[0] |
11 | RESERVED | PLL_PDN | RESERVED | RESERVED | RESERVED | RESERVED | AUTOSTRT | RESERVED |
14 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | 1 | RESERVED | 1 |
15 | RESERVED | XO_CAPCTRL[1] | XO_CAPCTRL[0] | XO_CAPCTRL[9] | XO_CAPCTRL[8] | XO_CAPCTRL[7] | XO_CAPCTRL[6] | XO_CAPCTRL[5] |
16 | XO_CAPCTRL[4] | XO_CAPCTRL[3] | XO_CAPCTRL[2] | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
19 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | OUT_SEL[2] |
20 | OUT_SEL[1] | OUT_SEL[0] | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
21 | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
22 | PLL_NDIV[11] | PLL_NDIV[10] | PLL_NDIV[9] | PLL_NDIV[8] | PLL_NDIV[7] | PLL_NDIV[6] | PLL_NDIV[5] | PLL_NDIV[4] |
23 | PLL_NDIV[3] | PLL_NDIV[2] | PLL_NDIV[1] | PLL_NDIV[0] | PLL_NUM[21] | PLL_NUM[20] | PLL_NUM[19] | PLL_NUM[18] |
24 | PLL_NUM[17] | PLL_NUM[16] | PLL_NUM[15] | PLL_NUM[14] | PLL_NUM[13] | PLL_NUM[12] | PLL_NUM[11] | PLL_NUM[10] |
25 | PLL_NUM[9] | PLL_NUM[8] | PLL_NUM[7] | PLL_NUM[6] | PLL_NUM[5] | PLL_NUM[4] | PLL_NUM[3] | PLL_NUM[2] |
26 | PLL_NUM[1] | PLL_NUM[0] | PLL_DEN[21] | PLL_DEN[20] | PLL_DEN[19] | PLL_DEN[18] | PLL_DEN[17] | PLL_DEN[16] |
27 | PLL_DEN[15] | PLL_DEN[14] | PLL_DEN[13] | PLL_DEN[12] | PLL_DEN[11] | PLL_DEN[10] | PLL_DEN[9] | PLL_DEN[8] |
28 | PLL_DEN[7] | PLL_DEN[6] | PLL_DEN[5] | PLL_DEN[4] | PLL_DEN[3] | PLL_DEN[2] | PLL_DEN[1] | PLL_DEN[0] |
29 | PLL_ DTHRMODE[1] |
PLL_DTHRMODE[0] | PLL_ORDER[1] | PLL_ORDER[0] | RESERVED | RESERVED | PLL_D | PLL_CP[3] |
30 | PLL_CP[2] | PLL_CP[1] | PLL_CP[0] | PLL_CP_PHASE_ SHIFT[2] |
PLL_CP_PHASE_ SHIFT[1] |
PLL_CP_PHASE_ SHIFT[0] |
PLL_ENABLE_ C3[2] |
PLL_ENABLE_ C3[1] |
31 | PLL_ENABLE_ C3[0] |
PLL_LF_R2[7] | PLL_LF_R2[6] | PLL_LF_R2[5] | PLL_LF_R2[4] | PLL_LF_R2[3] | PLL_LF_R2[2] | PLL_LF_R2[1] |
32 | PLL_LF_R2[0] | PLL_LF_C1[2] | PLL_LF_C1[1] | PLL_LF_C1[0] | PLL_LF_R3[6] | PLL_LF_R3[5] | PLL_LF_R3[4] | PLL_LF_R3[3] |
33 | PLL_LF_R3[2] | PLL_LF_R3[1] | PLL_LF_R3[0] | PLL_LF_C3[2] | PLL_LF_C3[1] | PLL_LF_C3[0] | RESERVED | RESERVED |
34 | RESERVED | OUT_DIV[8] | OUT_DIV[7] | OUT_DIV[6] | OUT_DIV[5] | OUT_DIV[4] | OUT_DIV[3] | OUT_DIV[2] |
35 | OUT_DIV[1] | OUT_DIV[0] | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
The default/reset values for each register is specified for LMK61E2-I3.
Name | Addr | Reset | Bit7 | Bit6 | Bit5 | Bit4 | Bit3 | Bit2 | Bit1 | Bit0 |
---|---|---|---|---|---|---|---|---|---|---|
VNDRID_BY1 | 0 | 0x10 | VNDRID[15:8] | |||||||
VNDRID_BY0 | 1 | 0x0B | VNDRID[7:0] | |||||||
PRODID | 2 | 0x33 | PRODID[7:0] | |||||||
REVID | 3 | 0x00 | REVID[7:0] | |||||||
SLAVEADR | 8 | 0xB0 | SLAVEADR[7:1] | RESERVED | ||||||
EEREV | 9 | 0x00 | EEREV[7:0] | |||||||
DEV_CTL | 10 | 0x01 | RESERVED | PLL_PDN | RESERVED | ENCAL | AUTOSTRT | |||
XO_CAPCTRL_ BY1 |
16 | 0x00 | RESERVED | XO_CAPCTRL[1:0] | ||||||
XO_CAPCTRL_ BY0 |
17 | 0x00 | XO_CAPCTRL[9:2] | |||||||
DIFFCTL | 21 | 0x01 | DIFF_OUT_PD | RESERVED | OUT_SEL[1:0] | |||||
OUTDIV_BY1 | 22 | 0x00 | RESERVED | OUT_DIV[8] | ||||||
OUTDIV_BY0 | 23 | 0x20 | OUT_DIV[7:0] | |||||||
PLL_NDIV_BY1 | 25 | 0x00 | RESERVED | PLL_NDIV[11:8] | ||||||
PLL_NDIV_BY0 | 26 | 0x64 | PLL_NDIV[7:0] | |||||||
PLL_FRACNUM_ BY2 |
27 | 0x00 | RESERVED | PLL_NUM[21:16] | ||||||
PLL_FRACNUM_ BY1 |
28 | 0x00 | PLL_NUM[15:8] | |||||||
PLL_FRACNUM_ BY0 |
29 | 0x00 | PLL_NUM[7:0] | |||||||
PLL_FRACDEN_ BY2 |
30 | 0x00 | RESERVED | PLL_DEN[21:16] | ||||||
PLL_FRACDEN_ BY1 |
31 | 0x00 | PLL_DEN[15:8] | |||||||
PLL_FRACDEN_ BY0 |
32 | 0x00 | PLL_DEN[7:0] | |||||||
PLL_MASHCTRL | 33 | 0x0C | RESERVED | PLL_DTHRMODE[1:0] | PLL_ORDER[1:0] | |||||
PLL_CTRL0 | 34 | 0x24 | RESERVED | PLL_D | RESERVED | PLL_CP[3:0] | ||||
PLL_CTRL1 | 35 | 0x03 | RESERVED | PLL_CP_PHASE_SHIFT[2:0] | RESERVED | PLL_ENABLE_C3[2:0] | ||||
PLL_LF_R2 | 36 | 0x28 | PLL_LF_R2[7:0] | |||||||
PLL_LF_C1 | 37 | 0x00 | RESERVED | PLL_LF_C1[2:0] | ||||||
PLL_LF_R3 | 38 | 0x00 | RESERVED | PLL_LF_R3[6:0] | ||||||
PLL_LF_C3 | 39 | 0x00 | RESERVED | PLL_LF_C3[2:0] | ||||||
PLL_CALCTRL | 42 | 0x00 | RESERVED | PLL_CLSDWAIT[1:0] | PLL_VCOWAIT[1:0] | |||||
NVMSCRC | 47 | 0x00 | NVMSCRC[7:0] | |||||||
NVMCNT | 48 | 0x00 | NVMCNT[7:0] | |||||||
NVMCTL | 49 | 0x10 | RESERVED | REGCOMMIT | NVMCRCERR | NVMAUTOCRC | NVMCOMMIT | NVMBUSY | NVMERASE | NVMPROG |
NVMLCRC | 50 | 0x00 | NVMLCRC[7:0] | |||||||
MEMADR | 51 | 0x00 | RESERVED | MEMADR[6:0] | ||||||
NVMDAT | 52 | 0x00 | NVMDAT[7:0] | |||||||
RAMDAT | 53 | 0x00 | RAMDAT[7:0] | |||||||
NVMUNLK | 56 | 0x00 | NVMUNLK[7:0] | |||||||
INT_LIVE | 66 | 0x00 | RESERVED | LOL | CAL | |||||
SWRST | 72 | 0x00 | RESERVED | SWR2PLL | RESERVED |
VNDRID_BY1 and VNDRID_BY0 registers are used to store the unique 16-bit Vendor Identification number assigned to I2C vendors.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | VNDRID[15:8] | R | 0x10 | N | Vendor Identification Number Byte 1. |
VNDRID_BY1 and VNDRID_BY0 registers are used to store the unique 16-bit Vendor Identification number assigned to I2C vendors.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | VNDRID[7:0] | R | 0x0B | N | Vendor Identification Number Byte 0. |
The Product Identification Number is a unique 8-bit identification number used to identify the LMK61E2.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | PRODID[7:0] | R | 0x33 | N | Product Identification Number. |
The REVID register is used to identify the LMK61E2 mask revision.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | REVID[7:0] | R | 0x00 | N | Device Revision Number. The Device Revision Number is used to identify the LMK61E2 mask-set revision used to fabricate this device. |
The SLAVEADR register reflects the 7-bit I2C Slave Address value initialized from from on-chip EEPROM.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7:1] | SLAVEADR[7:1] | R | 0x58 | Y | I2C Slave Address. This field holds the 7-bit Slave Address used to identify this device during I2C transactions. The two least significant bits of the address can be configured using ADD pin as shown. | |
SLAVEADR[2:1] | ADD pin | |||||
0 (0x0) | 0 | |||||
1 (0x1) | Float | |||||
3 (0x3) | 1 | |||||
[0] | RESERVED | - | - | N | Reserved. |
The EEREV register provides an EEPROM image revision record. EEPROM Image Revision is automatically retrieved from EEPROM and stored in the EEREV register after a reset or after a EEPROM commit operation.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | EEREV[7:0] | R | 0x00 | Y | EEPROM Image Revision ID |
The DEV_CTL register holds the control functions described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7] | RESERVED | - | 0 | Y | Reserved. | |
[6] | PLL_PDN | RW | 0 | Y | PLL Powerdown. The PLL_PDN bit determines whether PLL is automatically enabled and calibrated after a hardware reset. If the PLL_PDN bit is set to 1 during normal operation then PLL is disabled and the calibration circuit is reset. When PLL_PDN is then cleared to 0 PLL is re-enabled and the calibration sequence is automatically restarted. | |
PLL_PDN | Value | |||||
0 | PLL Enabled | |||||
1 | PLL Disabled | |||||
[5:2] | RESERVED[5:2] | RW | 0 | Y | Reserved. | |
[1] | ENCAL | RWSC | 0 | N | Enable Frequency Calibration. Triggers PLL/VCO calibration on both PLLs in parallel on 0 –> 1 transition of ENCAL. This bit is self-clearing and set to a 0 after PLL/VCO calibration is complete. In powerup or software rest mode, AUTOSTRT takes precedence. | |
[0] | AUTOSTRT | RW | 1 | Y | Autostart. If AUTOSTRT is set to 1 the device will automatically attempt to achieve lock and enable outputs after a device reset. A device reset can be triggered by the power-on-reset, RESETn pin or by writing to the RESETN_SW bit. If AUTOSTRT is 0 then the device will halt after the configuration phase, a subsequent write to set the AUTOSTRT bit to 1 will trigger the PLL Lock sequence. |
XO Margining Offset Value bits[9:8]
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:2] | RESERVED[5:0] | - | - | N | Reserved. |
[1:0] | XO_CAPCTRL [1:0] | RW | 0x0 | Y | XO Offset Value bits [1:0] |
XO margining Offset Value bits[7:0]
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | XO_CAPCTRL [9:2] | RW | 0x80 | Y | XO Offset Value bits[9:2] |
The DIFFCTL register provides control over Output.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7] | DIFF_OUT_PD | RW | 0 | N | Power down differential output buffer. | |
[6:2] | RESERVED | - | - | N | Reserved. | |
[1:0] | OUT_SEL[1:0] | RW | 0x1 | Y | Channel Output Driver Format Select. The OUT_SEL field controls the Channel Output Driver as shown below. | |
OUT_SEL | OUTPUT OPERATION | |||||
0 (0x0) | Tri-State | |||||
1 (0x1) | LVPECL | |||||
2 (0x2) | LVDS | |||||
3 (0x3) | HCSL |
The 9-bit output integer divider value is set by the OUTDIV_BY1 and OUTDIV_BY0 registers.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7:1] | RESERVED | RW | 0x00 | Y | Reserved. | |
[0] | OUT_DIV[8] | RW | 0 | Y | Channel's Output Divider Byte 1 (Bit 8). The Channel Divider, OUT_DIV, is a 9-bit divider. The valid values for OUT_DIV range from 5 to 511 as shown below. | |
OUT_DIV | DIVIDE RATIO | |||||
0-4 | RESERVED | |||||
5 (0x005) | 5 | |||||
6 (0x006) | 6 | |||||
7 (0x007) | 7 | |||||
255 (0x0FF) | 255 | |||||
256 (0x100) | 256 | |||||
257 (0x101) | 257 | |||||
... | ... | |||||
511 (0x1FF) | 511 |
The 9-bit output integer divider value is set by the OUTDIV_BY1 and OUTDIV_BY0 registers.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | OUT_DIV[7:0] | RW | 0x20 | Y | Channel's Output Divider Byte 0 (Bits 7-0). |
The 12-bit N integer divider value for PLL is set by the PLL_NDIV_BY1 and PLL_NDIV_BY0 registers.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:4] | RESERVED | - | - | N | Reserved. |
[3:0] | PLL_NDIV[11:8] | RW | 0x0 | Y | PLL N Divider Byte 1. PLL Integer N Divider bits [11:8]. |
The PLL_NDIV_BY0 register is described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | PLL_NDIV[7:0] | RW | 0x32 | Y | PLL N Divider Byte 0. PLL Integer N Divider bits [7:0]. |
The 22-bit Fractional Divider Numerator value for PLL is set by registers PLL_FRACNUM_BY2, PLL_FRACNUM_BY1 and PLL_FRACNUM_BY0.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:6] | RESERVED | - | - | N | Reserved. |
[5:0] | PLL_NUM[21:16] | RW | 0x00 | Y | PLL Fractional Divider Numerator Byte 2. Bits [21:16] |
The PLL_FRACNUM_BY1 register is described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | PLL_NUM[15:8] | RW | 0x00 | Y | PLL Fractional Divider Numerator Byte 1. Bits [15:8]. |
The PLL_FRACNUM_BY0 register is described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | PLL_NUM[7:0] | RW | 0x00 | Y | PLL Fractional Divider Numerator Byte 0. Bits [7:0]. |
The 22-bit Fractional Divider Denominator value for PLL is set by registers PLL_FRACDEN_BY2, PLL_FRACDEN_BY1 and PLL_FRACDEN_BY0.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:6] | RESERVED | - | - | N | Reserved. |
[5:0] | PLL_DEN[21:16] | RW | 0x00 | Y | PLL Fractional Divider Denominator Byte 2. Bits [21:16]. |
The PLL_FRACDEN_BY1 register is described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | PLL_DEN[15:8] | RW | 0x00 | Y | PLL Fractional Divider Denominator Byte 1. Bits [15:8]. |
The PLL_FRACDEN_BY0 register is described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | PLL_DEN[7:0] | RW | 0x00 | Y | PLL Fractional Divider Denominator Byte 0. Bits [7:0]. |
The PLL_MASHCTRL register provides control of the fractional divider for PLL.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7:4] | RESERVED | - | - | N | Reserved. | |
[3:2] | PLL_DTHRMODE[1:0] | RW | 0x3 | Y | Mash Engine dither mode control. | |
DITHERMODE | Dither Configuration | |||||
0 (0x0) | Weak | |||||
1 (0x1) | Reserved | |||||
2 (0x2) | Reserved | |||||
3 (0x3) | Dither Disabled | |||||
[1:0] | PLL_ORDER[1:0] | RW | 0x0 | Y | Mash Engine Order. | |
ORDER | Order Configuration | |||||
0 (0x0) | Integer Mode Divider | |||||
1 (0x1) | Reserved | |||||
2 (0x2) | Reserved | |||||
3 (0x3) | 3rd order |
The PLL_CTRL1 register provides control of PLL. The PLL_CTRL1 register fields are described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7:6] | RESERVED | RW | 0x0 | Y | Reserved. | |
[5] | PLL_D | RW | 1 | Y | PLL R Divider Frequency Doubler Enable. If PLL_D is 1 the R Divider Frequency Doubler is enabled. | |
[4] | RESERVED | - | - | N | Reserved. | |
[3:0] | PLL_CP[3:0] | RW | 0x8 | Y | PLL Charge Pump Current. Other combinations of PLL_CP[3:0] not in table below are reserved and not supported. | |
PLL_CP[3:0] | PLL Charge Pump Current | |||||
4 (0x4) | 1.6 mA | |||||
8 (0x8) | 6.4 mA |
The PLL_CTRL3 register provides control of PLL. The PLL_CTRL3 register fields are described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7] | RESERVED | - | - | N | Reserved. | |
[6:4] | PLL_CP_PHASE_SHIFT[2:0] | RW | 0x0 | Y | Program Charge Pump Phase Shift. | |
PLL_CP_PHASE_SHIFT[2:0] | Phase Shift | |||||
0 (0x0) | No delay | |||||
1 (0x1) | 1.3 ns for 100 MHz fPD | |||||
2 (0x2) | 1 ns for 100 MHz fPD | |||||
3 (0x3) | 0.9 ns for 100 MHz fPD | |||||
4 (0x4) | 1.3 ns for 50 MHz fPD | |||||
5 (0x5) | 1 ns for 50 MHz fPD | |||||
6 (0x6) | 0.9 ns for 50 MHz fPD | |||||
7 (0x7) | 0.7 ns for 50 MHz fPD | |||||
[3] | RESERVED | - | - | N | Reserved. | |
[2] | PLL_ENABLE_C3 | RW | 0 | Y | Disable third order capacitor in the low pass filter. | |
PLL_ENABLE_C3 | MODE | |||||
0 | 2nd order loop filter recommended setting | |||||
1 | Enables C3, 3rd order loop filter enabled | |||||
[1:0] | RESERVED | - | 0x3 | Y | Reserved. |
The PLL_LF_R2 register controls the value of the PLL Loop Filter R2.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7:0] | PLL_LF_R2[7:0] | RW | 0x08 | Y | PLL Loop Filter R2. NOTE: Table below lists commonly used R2 values but more selections are available. | |
PLL_LF_R2[7:0] | R2 (Ω) | |||||
1 (0x01) | 200 | |||||
4 (0x04) | 500 | |||||
8 (0x08) | 700 | |||||
32 (0x20) | 1600 | |||||
48 (0x30) | 2400 | |||||
64 (0x40) | 3200 |
The PLL_LF_C1 register controls the value of the PLL Loop Filter C1.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:3] | RESERVED | - | - | N | Reserved. |
[2:0] | PLL_LF_C1[2:0] | RW | 0x0 | Y | PLL Loop Filter C1. The value in pF is given by 5 + 50 * PLL_LF_C1 (in decimal). |
The PLL_LF_R3 register controls the value of the PLL Loop Filter R3.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7] | RESERVED | - | - | N | Reserved. | |
[6:0] | PLL_LF_R3[6:0] | RW | 0x00 | Y | PLL Loop Filter R3. NOTE: Table below lists commonly used R3 values but more selections are available. | |
PLL_LF_R3[6:0] | R3 (Ω) | |||||
0 (0x00) | 18 | |||||
3 (0x03) | 205 | |||||
8 (0x08) | 854 | |||||
9 (0x09) | 1136 | |||||
12 (0x0C) | 1535 | |||||
17 (0x11) | 1936 | |||||
20 (0x14) | 2335 |
The PLL_LF_C3 register controls the value of the PLL Loop Filter C3.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:3] | RESERVED | - | - | N | Reserved. |
[2:0] | PLL_LF_C3[2:0] | RW | 0x0 | Y | PLL Loop Filter C3. The value in pF is given by 5 * PLL_LF_C3 (in decimal). |
The PLL_CALCTRL register is described in the following table.
Bit # | Field | Type | Reset | EEPROM | Description | |
---|---|---|---|---|---|---|
[7:4] | RESERVED | - | - | N | Reserved. | |
[3:2] | PLL_CLSDWAIT[1:0] | RW | 0x2 | Y | Closed Loop Wait Period. The CLSDWAIT field sets the closed loop wait period. Recommended value is 0x2. | |
CLSDWAIT | Anlog closed loop VCO stabilization time | |||||
0 (0x0) | 150 µs | |||||
1 (0x1) | 300 µs | |||||
2 (0x2) | 500 µs | |||||
3 (0x3) | 2000 µs | |||||
[1:0] | PLL_VCOWAIT[1:0] | RW | 0x1 | Y | VCO Wait Period. Recommended value is 0x1. | |
VCOWAIT | VCO stabilization time | |||||
0 (0x0) | 20 µs | |||||
1 (0x1) | 400 µs | |||||
2 (0x2) | 4000 µs | |||||
3 (0x3) | 10000 µs |
The NVMSCRC register holds the Stored CRC (Cyclic Redundancy Check) byte that has been retreived from on-chip EEPROM.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | NVMSCRC[7:0] | R | 0x00 | Y | EEPROM Stored CRC. |
The NVMCNT register is intended to reflect the number of on-chip EEPROM Erase/Program cycles that have taken place in EEPROM. The count is automatically incremented by hardware and stored in EEPROM.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | NVMCNT[7:0] | R | 0x00 | Y | EEPROM Program Count. The NVMCNT increments automatically after every EEPROM Erase/Program Cycle. The NVMCNT value is retreived automatically after reset, after a EEPROM Commit operation or after a Erase/Program cycle. The NVMCNT register will increment until it reaches its maximum value of 255 after which no further increments will take place. |
The NVMCTL register allows control of the on-chip EEPROM Memories.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7] | RESERVED | - | - | N | Reserved. |
[6] | REGCOMMIT | RWSC | 0 | N | REG Commit to EEPROM SRAM Array. The REGCOMMIT bit is used to initiate a transfer from the on-chip registers back to the corresponding location in the EEPROM SRAM Array. The REGCOMMIT bit is automatically cleared to 0 when the transfer is complete. |
[5] | NVMCRCERR | R | 0 | N | EEPROM CRC Error Indication. The NVMCRCERR bit is set to 1 if a CRC Error has been detected when reading back from on-chip EEPROM during device configuration. |
[4] | NVMAUTOCRC | RW | 1 | N | EEPROM Automatic CRC. When NVMAUTOCRC is 1 then the EEPROM Stored CRC byte is automatically calculated whenever a EEPROM program takes place. |
[3] | NVMCOMMIT | RWSC | 0 | N | EEPROM Commit to Registers. The NVMCOMMIT bit is used to initiate a transfer of the on-chip EEPROM contents to internal registers. The transfer happens automatically after reset or when NVMCOMMIT is set to 1. The NVMCOMMIT bit is automatically cleared to 0. The I2C registers cannot be read while a EEPROM Commit operation is taking place. |
[2] | NVMBUSY | R | 0 | N | EEPROM Program Busy Indication. The NVMBUSY bit is 1 during an on-chip EEPROM Erase/Program cycle. While NVMBUSY is 1 the on-chip EEPROM cannot be accessed. |
[1] | NVMERASE | RWSC | 0 | N | EEPROM Erase Start. The NVMERASE bit is used to begin an on-chip EEPROM Erase cycle. The Erase cycle is only initiated if the immediately preceding I2C transaction was a write to the NVMUNLK register with the appropriate code. The NVMERASE bit is automatically cleared to 0. The EEPROM Erase operation takes around 115ms. |
[0] | NVMPROG | RWSC | 0 | N | EEPROM Program Start. The NVMPROG bit is used to begin an on-chip EEPROM Program cycle. The Program cycle is only initiated if the immediately preceding I2C transaction was a write to the NVMUNLK register with the appropriate code. The NVMPROG bit is automatically cleared to 0. If the NVMERASE and NVMPROG bits are set simultaneously then an ERASE/PROGRAM cycle will be executed The EEPROM Program operation takes around 115ms. |
The MEMADR register holds 7-bits of the starting address for on-chip SRAM or EEPROM access.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7] | RESERVED | - | - | N | Reserved. |
[6:0] | MEMADR[6:0] | RW | 0x00 | N | Memory Address. The MEMADR value determines the starting address for on-chip SRAM read/write access or on-chip EEPROM access. The internal address to access SRAM or EEPROM is automatically incremented; however the MEMADR register does not reflect the internal address in this way. When the SRAM or EEPROM arrays are accessed using the I2C interface only bits [4:0] of MEMADR are used to form the byte Wise address. |
The NVMDAT register returns the on-chip EEPROM contents from the starting address specified by the MEMADR register.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | NVMDAT[7:0] | R | 0x00 | N | EEPROM Read Data. The first time an I2C read transaction accesses the NVMDAT register address, either because it was explicitly targeted or because the address was auto-incremented, the read transaction will return the EEPROM data located at the address specified by the MEMADR register. Any additional read's which are part of the same transaction will cause the EEPROM address to be incremented and the next EEPROM data byte will be returned. The I2C address will no longer be auto-incremented, i.e the I2C address will be locked to the NVMDAT register after the first access. Access to the NVMDAT register will terminate at the end of the current I2C transaction. |
The RAMDAT register provides read and write access to the SRAM that forms part of the on-chip EEPROM module.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | RAMDAT[7:0] | RW | 0x00 | N | RAM Read/Write Data. The first time an I2C read or write transaction accesses the RAMDAT register address, either because it was explicitly targeted or because the address was auto-incremented, a read transaction will return the RAM data located at the address specified by the MEMADR register and a write transaction will cause the current I2C data to be written to the address specified by the MEMADR register. Any additional accesses which are part of the same transaction will cause the RAM address to be incremented and a read or write access will take place to the next SRAM address. The I2C address will no longer be auto-incremented, i.e the I2C address will be locked to the RAMDAT register after the first access. Access to the RAMDAT register will terminate at the end of the current I2C transaction. |
The NVMUNLK register provides a rudimentary level of protection to prevent inadvertent programming of the on-chip EEPROM.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:0] | NVMUNLK[7:0] | RW | 0x00 | N | EEPROM Prog Unlock. The NVMUNLK register must be written immediately prior to setting the NVMPROG bit of register NVMCTL, otherwise the Erase/Program cycle will not be triggered. NVMUNLK must be written with a value of 0xBE. |
The INT_LIVE register reflects the current status of the interrupt sources.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:2] | RESERVED | - | - | N | Reserved. |
[1] | LOL | R | 0 | N | Loss of Lock PLL. |
[0] | CAL | R | 0 | N | Calibration Active PLL. |
The SWRST1 register provides software reset control for specific on-chip modules. Each bit in this register is individually self cleared after a write operation. The SWRST1 register will always return 0x00 in a read transaction.
Bit # | Field | Type | Reset | EEPROM | Description |
---|---|---|---|---|---|
[7:2] | RESERVED | - | - | N | Reserved. |
[1] | SWR2PLL | RWSC | 0 | N | Software Reset PLL. Setting SWR2PLL to 1 resets the PLL calibrator and clock dividers. This bit is automatically cleared to 0. |
[0] | RESERVED | - | - | N | Reserved. |