JAJSOI8H November 2009 – May 2022 LMP8645 , LMP8645HV
PRODUCTION DATA
The maximum voltage at the RG pin is Vout_max, it means that:
where
So all the RGAIN resistors which respect the previous inequality are allowed. The graphical representation in Figure 7-5 helps with the selection.
All the combinations (VSENSE, RGAIN) below the curves are allowed.
Also in this range once selected the RGAIN (Gain) the VSENSE range is fixed too.
From the ranges shown above, a good way to maximize the output voltage swing of the LMP8645 is to select the maximum allowable RGAIN according to the previous equations. For a fixed supply voltage and VSENSE as the common-mode voltage increases, the maximum allowable RGAIN increases too.