JAJSF93 April 2018 LMV7239-Q1
PRODUCTION DATA.
A window detector monitors the input signal to determine if it falls between two voltage levels. Both outputs are true (high) when VREF1< VIN < VREF2
The comparator outputs A and B are high only when VREF1< VIN < VREF2, or "within the window", where these are defined as:
To determine if the input signal falls outside of the two voltage levels, both inputs on each comparators can be reversed to invert the logic.
Other names for window detectors are: threshold detector, level detector, and amplitude trigger or detector.