JAJSH78J June 2010 – April 2019 LMZ10503EXT
PRODUCTION DATA.
Alternatively, the tracking feature can be used to have similar output voltage ramp rates. This is referred to as simultaneous start-up. In this case, the tracking resistors can be determined based on Equation 5:
and to ensure proper overdrive of the SS pin:
For the example case of VOUT1 = 5 V and VOUT2 = 2.5 V, with Rtrkt set to 33 kΩ as before, Rtrkb is calculated from Equation 5 to be 15.5 kΩ. Figure 20 shows an example of tracking using equal slew rates.