JAJSBZ7E JULY 2013 – December 2019 LMZ31710
PRODUCTION DATA.
The LMZ31710 is designed to operate from an input voltage supply range between 2.95 V and 17 V. This input supply should be well regulated and able to withstand maximum input current and maintain a stable voltage. The resistance of the input supply rail should be low enough that an input current transient does not cause a high enough drop at the supply voltage that can cause a false UVLO fault triggering and system reset.
If the input supply is located more than a few inches from the LMZ31710, additional bulk capacitance may be required at the input pins. A typical recommended amount of bulk input capacitance is 47 μF - 100 μF.