JAJSHN1A June 2019 – August 2019 LP8867-Q1 , LP8869-Q1
PRODUCTION DATA.
The output current of the LED outputs is controlled with external RISET resistor. RISET value for the target LED current per channel can be calculated using Equation 5:
where
For example, if RISET is set to 20 kΩ, ILED will be 120 mA per channel.