JAJSHN1A June 2019 – August 2019 LP8867-Q1 , LP8869-Q1
PRODUCTION DATA.
The LP886x-Q1 has a power-line FET control feature. It has a control pin (SD) for driving the gate of an external power-line P-Channel MOSFET. This feature grants LP886x-Q1 the ability to immediately cut-off the power part of backlight system when failure occurs, protecting other parallel power systems from being impacted. In addition, the feature could smooth the inrush current during powering-up by turning on the power-line FET gradually. In SOFT START state, the SD pin slowly increases the sink current until it reaches 230 μA. An example schematic is shown in Figure 14.
The value of RGS should follow the rules below
A 20-kΩ RGS is chosen in typical application which generates a 4.6 V difference on power-line FET's Source-Gate voltage.
The LP886x-Q1 turns off the power-line FET and prevents the possible boost and LEDs leakage when the device is disabled or in FAULT RECOVERY state.
Power-line FET control is an optional feature. Leave SD pin NC and don't use power-line FET when this feature is not needed.