JAJSHN1A June 2019 – August 2019 LP8867-Q1 , LP8869-Q1
PRODUCTION DATA.
The LP886x-Q1 has an optional feature to decrease automatically LED current when LED overheating is detected with an external NTC sensor. An example of the behavior is shown in Figure 15. When the NTC temperature reaches T1, the LP886x-Q1 starts to decrease the LED current. When the LED current has reduced to 17.5% of the nominal value, current turns off until temperature returns to the operation range.
Figure 15. Temperature-Based LED Current Dimming Functionality
Figure 16. Temperature-Based LED Current Dimming Implementation When TSET pin is grounded and TSENSE is floated, this feature is disabled. LED current is set by RISET resistor:
where
When external NTC is connected, the TSENSE pin current decreases LED output current. Temperature T1 and de-rate slope are defined by external resistors as explained below.
Parallel resistance of the NTC sensor RT and resistor R4 is calculated by formula:
TSET voltage can be calculated with Equation 8:
TSENSE pin current is calculated by Equation 9:
where
ISET pin current defined by RISET is:
For Equation 11, ITSENSE current must be limited between 0 and ISET_SCALED. If ITSENSE > ISET_SCALED then set ITSENSE = ISET_SCALED. If ITSENSE < 0 then set ITSENSE = 0.
LED driver output current is:
When current is lower than 17.5% of the nominal value, the current is set to 0 (the cut-off point).
An Excel® calculator is available for calculating the component values for a specific NTC and target thermal profile (contact TI E2E™ support forums ). Figure 17 shows an example thermal profile implementation.
| NTC – 10 kΩ at 25ºC | RISET = 24 kΩ | R2 = 10 kΩ | R4 = 100 kΩ |
| VDD = 4.3 V | R1 = 10 kΩ | R3 = 2 kΩ | R5 = 7.5 kΩ |