JAJSS82E August 2009 – July 2024 LPV521
PRODUCTION DATA
The amplifier differential inputs consist of a noninverting input (+IN) and an inverting input (–IN). The amplifier amplifies only the difference in voltage between the two inputs, which is called the differential input voltage. The output voltage of the op-amp VOUT is given by Equation 1:
where AOL is the open-loop gain of the amplifier, typically around 132dB (4,000,000 ×, or 0.25µV/V).