JAJSST7A January 2024 – May 2024 MCF8315C-Q1
PRODUCTION DATA
The DC bus current limit feature can be used to limit the current supplied by the DC input source (VM). This feature can be enabled by setting BUS_CURRENT_LIMIT_ENABLE to 1b. The DC bus current limit can be configured using BUS_CURRENT_LIMIT. This feature limits the DC bus current by limiting the speed (SPEED_REF_LIM)/current (CURRENT_REF_LIM) reference as shown in Figure 6-49. Enabling this feature may restrict the speed/phase current of the motor from reaching the set point (SPEED_REF or CURRENT_REF) in order to limit the DC bus current. The DC bus current limit status is reported on BUS_CURRENT_LIMIT_STATUS.