JAJSOP2 December 2022 OPT3005
PRODUCTION DATA
To communicate with the OPT3005, the host must first initiate an I2C start command. Then, the host must address sensor devices via a sensor address byte. The sensor address byte consists of seven address bits and a direction bit that indicates whether the action is to be a read or write operation.
Four I2C addresses are possible by connecting the ADDR pin to one of four pins: GND, VDD, SDA, or SCL. Table 8-1 summarizes the possible addresses with the corresponding ADDR pin configuration. The state of the ADDR pin is sampled on every bus communication and must be driven or connected to the desired level before any activity on the interface occurs.
DEVICE I2C ADDRESS | ADDR PIN |
---|---|
1000100 | GND |
1000101 | VDD |
1000110 | SDA |
1000111 | SCL |