JAJSUM7 May 2024 PCM1841-Q1
ADVANCE INFORMATION
The device record channel includes a high dynamic range and built-in digital decimation filter to process the oversampled data from the multibit delta-sigma (ΔΣ) modulator, which generates digital data at the same Nyquist sampling rate as the FSYNC rate. The decimation filter can be chosen from Section 6.3.7.2.1 and Section 6.3.7.2.2 only in target mode, depending on the required frequency response, group delay, and phase linearity requirements for the target application. The MD0 pin can select the decimation filter option. Table 6-7 shows the decimation filter mode selection for the record channel.
MD0 | DECIMATION FILTER MODE SELECTION (Supported Only in Target Mode) |
---|---|
LOW | Linear phase filters are used for the decimation in target mode. For controller mode, the device always uses linear phase filters for the decimation. |
HIGH | Low latency filters are used for the decimation in target mode. For controller mode, the device always uses linear phase filters for the decimation. |