JAJSKP5A December 2020 – September 2021 TAS2764
PRODUCTION DATA
Brownout Prevention (BOP) feature provides a priority input to the limiter to generate a fast response to transient dips in supply voltage at end of charge conditions that can cause system level brownout. When supply voltage dips below the BOP threshold, the limiter begins reducing gain at a configurable attack rate. When supply voltage rises above the BOP threshold, the limiter will begin to release after the programmed hold time. The BOP feature can be enabled by setting the BOP_EN register bit high. The brownout supply source can be set using BOP_SRC register bit to either PVDD (BOP_SRC =1) or VBAT1S (BOP_SRC =0) depending on application need. It should be noted that the BOP feature is independent of the limiter and will function, if enabled, even if the Supply Tracking Limiter is disabled.
The BOP can be configured to attack the gain through four levels as the supply voltage continues to drop. The BOP threshold Level 3 is set using the BOP_TH3[7:0] register bits followed by threshold Level 2 using BOP_TH2[7:0] register bits, Level 1 threshold set by BOP_TH1[7:0] bits and finally crossing Level 0 set by BOP_TH0[7:0] register bits.
The BOP levels that are not used can be disabled individually using register bits BOP_DIS0, BOP_DIS1, BOP_DIS2, BOP_DIS_3 and providing flexibility from one to four levels. Levels should be disabled in the order 3 to 1 for proper operation.
Each level has a separate Attack Rate (register bits BOP_ATK_RT0[2:0] to BOP_ATK_RT3[2:0]), Attack Step Size (register bits BOP_ATK_ST0[2:0] to BOP_ATK_ST3[2:0]), Release Rate (register bits BOP_RLS_RT0[2:0] to BOP_RLS_RT3[2:0]), Release Step Size (register bits BOP_RLS_ST0[3:0] to BOP_RLS_ST3[3:0]), Dwell Time (register bits BOP_DT0[2:0] to BOP_DT3[2:0]), Hold Time (register bits BOP_HT0[2:0] to BOP_HT3[2:0]), Maximum Attenuation and Shutdown.
When BOP supply source is set to PVDD input the SAR convertor will not digitize the VBAT1S voltage to reduce latency in the first attack of the BOP engine.
For proper device operation the following conditions must be met:
● BOP_MAX_ATTN0 > BOP_MAX_ATTN1 > BOP_MAX_ATTN2 > BOP_MAX_ATTN3
● BOP_TH Level 3 > BOP_TH Level 2 > BOP_TH Level 1 > BOP_TH Level 0.
Use bits BOP_MAX_ATTN of registers BOP_CFG4, BOP_CFG9, BOP_CFG14, BOP_CFG20 from Register Map to set attenuation levels. Registers BOP_CFG5, BOP_CFG10, BOP_CFG15, BOP_CFG21 will be used for setting the BOP threshold levels.
The TAS2764 can also immediately mute and then shutdown the device when a BOP event occurs by reaching Level 0 if the BOP_SHDN register bit is set high. For the device to continue playing audio again it must transition through a SW/HW shutdown state. If the hold time set by BOP_HT3[2:0] , BOP_HT2[2:0], BOP_HT1[2:0], BOP_HT0[2:0] register bits is at 7h (Infinite) the device needs to transition through a mute or SW/HW shutdown state or the register bit BOP_HLD_CLR can be set to high (which will cause the device to exit the hold state and begin releasing). This bit is self clearing and will always read-back low.
The TAS2764 BOP engine will keep track of the current level state, the lowest BOP level that has been engaged and the lowest sensed BOP supply voltage. This information is continually updated until requested. When this information is polled the register BOP_STAT_HLD is set high. This will pause the updates of the current state (BOP_STAT_STATE[3:0]) and lowest BOP level (BOP_STAT_LLVL[2:0]) registers bits allowing them to be read back. Once the read is complete the register bit BOP_STAT_HLD should be set low again clearing the current BOP status registers and re-enabling the updates based on current BOP state.
The lowest PVDD measurement since the last read is also available in register bits BOP_STAT_PVDD[9:0] if BOP_STAT_HLD register bit is set high before reading.
BOP Level 0 cannot be disabled and BOP Level 0 thresholds will be fixed by values programmed in registers 0x2E to 0x32 of page 0x00.