JAJSFI3A May 2018 – November 2018 TAS3251
PRODUCTION DATA.
The following is a sample script for using the DSP host memory to change the fine volume on the device on I2C slave address 0x90 to the default value of 0 dB:
w 90 00 00 #Go to page 0
w 90 7f 8C #Change the book to 0x8C
w 90 00 21 #Go to page 0x21
w 90 34 40 00 00 00 #Fine volume Left
w 90 38 40 00 00 00 #Fine volume Rights
#Run the swap flag for the DSP to work on the new coefficients
w 90 00 00 #Go to page 0
w 90 7f 8C #Change the book to 0x8C
w 90 00 05 #Go to page 0x05
w 90 7C 00 00 00 01 #Swap flag