JAJSFI3A May 2018 – November 2018 TAS3251
PRODUCTION DATA.
The input mixer can be used to mix the left and right channel input signals as shown in Figure 42. The input mixer has four coefficients, which control the mixing and gains of the input signals. When mixing and scaling the input signals, ensure that at maximum input level the input mixer outputs don't exceed 0 dBFs, which will overdrive the SRC inputs.