JAJSHZ2C January 2014 – September 2019 TCA5013
PRODUCTION DATA.
The card CLK pins have a current limiting feature that prevents excess current from being drawn on them. When an external load tries to draw a current higher than the limit, the device responds by adjusting the VOH or VOL to limit the current. The device does not deactivate the card interface when over current limit of the CLK pins are reached.