JAJSFN6G September 2009 – June 2018 TCA8418
PRODUCTION DATA.
The TCA8418 can support normal key presses, but it also can support a <Ctrl><Alt><Del> (CAD) key press. This feature allows the host to recognize a specific key press and alert the host that the combination has occurred. The TCA8418 will recognize a <Ctrl><Alt><Del> key press if keys 1, 11, and 21 are all pressed at the same time. These keys are referenced to the key values listed in the Key Event Table. Note that this key combination that triggers a CAD interrupt is not adjustable, and must be keys 1, 11, and 21.
Please see CAD Interrupt Errata for more information.